SparkFun Inventor's Kit Experiment Guide - v4.1

≡ Pages
Contributors: Joel_E_B, bboyho

SIK Printed Guidebook Errata

The following corrections list the errors and updates to the SIK printed Guidebook.

If you are having issues and notice an error in the latest version, please contact SparkFun's support team.

Corrections for V4.1.2 and V4.1

Please Note: All of these corrections have been made to the online version of the SIK Guide. To follow along with the digital guide, click on the link below.

SparkFun Inventor's Kit Experiment Guide - v4.1

August 8, 2019
The SparkFun Inventor's Kit (SIK) Experiment Guide contains all of the information needed to build all five projects, encompassing 16 circuits, in the latest version of the kit, v4.1.2 and v4.1.

Page 18

In the Code to Note, the code states that the digital output to turn on the LED is D13. While the physcial pin reference is correct, the "D" should not be used in code.

digitalWrite(D13, HIGH);

Make sure to remove the letter "D" for the input when turning on and off the pin.

digitalWrite(13, HIGH);

Page 73

The correct circuit diagram for circuit 4A is as follows:

Circuit 4A


Corrections for V4.0 to V4.0a

Please Note: All of these corrections have been made to the online version of the SIK Guide. To follow along with the digital guide, click on the link below.

SparkFun Inventor's Kit Experiment Guide - v4.0

November 15, 2017
The SparkFun Inventor's Kit (SIK) Experiment Guide contains all of the information needed to build all five projects, encompassing 16 circuits, in the latest version of the kit, v4.0a.

To download a printable PDF of this Errata sheet, click the link below.




Page 73

The correct circuit diagram for circuit 4A is as follows:

Circuit 4A

Page 82

The You Need parts list is missing a Buzzer, which is needed to build circuit 4C. The correct parts list is shown below.

4C Parts




Page 84

The circuit diagram is correct, however the coordinates listed for the Buzzer and the Jumper Wires that connect the Buzzer to the RedBoard are incorrect. The correct coordinates are:

Component RedBoard Breadboard Breadboard
Buzzer G6
(Buzzer +)
G8
(Buzzer -)
Jumper Wire Digital Pin 6 J6
Jumper Wire J8 GND Rail
( - )

Page 93

The correct circuit diagram for circuit 5A is as follows:

Circuit_5A

Changes made to the circuit diagram are also reflected in the hookup table revisions shown below.

Component RedBoard Breadboard
Jumper Wire Digital Pin 8 J5
Jumper Wire Digital Pin 9 J6
Jumper Wire Digital Pin 10 J7
Jumper Wire Digital Pin 11 J1
Jumper Wire Digital Pin 12 J2
Jumper Wire Digital Pin 13 J3

Please make sure that you are using the most up-to-date version of the SIK v4.0a code (SIK_Guide_Code-V_4.0a) with this diagram.

Page 98

The correct circuit diagram for circuit 5B is as follows:

Circuit_5B

Changes made to the circuit diagram are also reflected in the hookup table revisions shown below.

Component RedBoard Breadboard
Jumper Wire Digital Pin 8 J5
Jumper Wire Digital Pin 9 J6
Jumper Wire Digital Pin 10 J7
Jumper Wire Digital Pin 11 J1
Jumper Wire Digital Pin 12 J2
Jumper Wire Digital Pin 13 J3

Please make sure that you are using the most up-to-date version of the SIK v4.0a code (SIK_Guide_Code-V_4.0a) with this diagram.

Page 103

The correct circuit diagram for circuit 5C is as follows:

Circuit_5C

Changes made to the circuit diagram are also reflected in the hookup table revisions shown below.

Component RedBoard Breadboard
Jumper Wire Digital Pin 8 J5
Jumper Wire Digital Pin 9 J6
Jumper Wire Digital Pin 10 J7
Jumper Wire Digital Pin 11 J1
Jumper Wire Digital Pin 12 J2
Jumper Wire Digital Pin 13 J3

Please make sure that you are using the most up-to-date version of the SIK v4.0a code (SIK_Guide_Code-V_4.0a) with this diagram.

SIK Code

The changes made to Project 5's circuit diagrams also necessitate a change to the code for each circuit. Please make sure you are using the most up-to-date SIK code, which can be downloaded using the button below or at the following URL: www.sparkfun.com/SIKcode