Qwiic SHIM Kit for Raspberry Pi Hookup Guide

≡ Pages
Contributors: bboyho

Introduction

The Qwiic SHIM Kit for Raspberry Pi gets you started with some of the basics surrounding I2C and Python on your Raspberry Pi. This tutorial will go over connecting Qwiic-enabled devices, installing their Python packages, and running the example code.

SparkFun Qwiic SHIM Kit for Raspberry Pi

KIT-16987
Retired

Required Materials

To follow along with this tutorial, you will also need a few pieces of hardware. Single board computers with the Raspberry Pi 40-pin GPIO standard header will work. We'll be using a Raspberry Pi throughout this tutorial. If you have not worked with a Raspberry Pi, we recommend pairing the Qwiic SHIM Kit with a Raspberry Pi 4 kit. At a minimum, you'll need a basic kit. However, if you need keyboard and mouse combination, we recommend getting the desktop kit.

SparkFun Raspberry Pi 4 Basic Kit - 4GB

KIT-16384
Retired

SparkFun Raspberry Pi 4 Desktop Kit - 4GB

KIT-16386
Retired

Optional Materials

You have several options when it comes to working with the Raspberry Pi. Most commonly, the Pi is used as a standalone computer, which requires a monitor. The following parts can be used with the Pi 4 if you opt for a small display. To save on costs, the Pi can also be used as a headless computer (without a monitor, keyboard, and mouse). This setup has a slightly more difficult learning curve, as you will need to use the command-line interface (CLI) from another computer.

Raspberry Pi LCD - 7" Touchscreen

LCD-13733
$88.30

SmartiPi Touch 2

PRT-16302
Retired

Suggested Reading

If you aren't familiar with Qwiic, we recommend reading here for an overview.

Qwiic Connect System
Qwiic Connect System

We also recommend taking a look at some of our other tutorials and familiarizing yourself with some of these topics and parts. We will end up working with the Raspberry Pi and Python programming language.

Raspberry Pi 4 Kit Hookup Guide

March 14, 2020
Guide for hooking up your Raspberry Pi 4 Model B basic, desktop, or hardware starter kit together.

Python Programming Tutorial: Getting Started with the Raspberry Pi

June 27, 2018
This guide will show you how to write programs on your Raspberry Pi using Python to control hardware.

I2C

An introduction to I2C, one of the main embedded communications protocols in use today.

Serial Terminal Basics

This tutorial will show you how to communicate with your serial devices using a variety of terminal emulator applications.

AVR-Based Serial Enabled LCDs Hookup Guide

The AVR-based Qwiic Serial Enabled LCDs are a simple and cost effective solution to include in your project. These screens are based on the HD44780 controller, and include ATmega328P with an Arduino compatible bootloader. They accept control commands via Serial, SPI and I2C (via PTH headers or Qwiic connector). In this tutorial, we will show examples of a simple setup and go through each communication option.

SparkFun 9DoF IMU (ICM-20948) Breakout Hookup Guide

How to use the SparkFun 9DoF ICM-20948 breakout board for your motion sensing projects. This breakout is ideal for wearable sensors and IoT applications.

Qwiic SHIM for Raspberry Pi Hookup Guide

Ever wanted to prototype I2C components on a Pi? Now you can!