Qwiic Digital Indoor Thermometer

≡ Pages
Contributors: bboyho

Resources and Going Further

Well, that was quick! Depending on where you place your sensor, you may need to offset the temperature sensor reading. Try adding the Qwiic button and modifying the code to toggle between degrees Fahrenheit or Celsius rather than the scroll bar. Or try adding a few more Qwiic sensors to monitor your environment. Then try making an enclosure to protect your Qwiic tower of sensing power! Looking for inspiration? Check out these other great tutorials using Qwiic-enabled sensors from SparkFun.

CCS811/BME280 (Qwiic) Environmental Combo Breakout Hookup Guide

Sense various environmental conditions such as temperature, humidity, barometric pressure, eCO2 and tVOCs with the CCS811 and BME280 combo breakout board.

Qwiic Ambient Light Sensor (VEML6030) Hookup Guide

The VEML6030 is a high accuracy ambient light sensor with 16-bit resolution. This I2C sensor can detect light similar to the human eye response. Start detecting light levels in your environment!

Qwiic Atmospheric Sensor (BME280) Hookup Guide

Measure temperature, humidity, barometric pressure with the SparkFun Atmospheric Sensor Breakout BME280 (Qwiic).

SparkFun Humidity Sensor Breakout - SHTC3 (Qwiic) Hookup Guide

A Hookup Guide to get started using the SHTC3 breakout.

Looking for more temperature sensing fun? Check out the following tutorials with non-contact temperature sensors.

MLX90614 IR Thermometer Hookup Guide

How to use the MLX90614 or our SparkFun IR Thermometer Evaluation Board to take temperatures remotely, over short distances.

Qwiic GRID-Eye Infrared Array (AMG88xx) Hookup Guide

The Panasonic GRID-Eye (AMG88xx) 8x8 thermopile array serves as a functional low-resolution infrared camera. This means you have a square array of 64 pixels each capable of independent temperature detection. It’s like having thermal camera (or Predator’s vision), just in really low resolution.

Qwiic IR Array (MLX90640) Hookup Guide

The Melexis MLX90640 contains a 32x24 array of thermopile sensors creating, in essence, a low resolution thermal imaging camera. In this guide, we’ll go over how to connect your Qwiic Infrared Array with MLX90640 and get it communicating with Processing to produce a nice thermal image.