Photon Remote Water Level Sensor

≡ Pages
Contributors: wordsforthewise

Final Data Analysis

Here's some data from field testing:

light values during the day

Full Colorado sunlight is bright.

temperature during the day

The temp inside the box got up to about 95...when it was 60 out. May have to move this into the shade after all. There were also some strange gyrations going on.

battery SOC during the day

The battery never dropped below 40% over one night. I'm also running two ultrasonic sensors, which draws a bit more power.

pressure change during the day

The pressure was dropping in the 'moderate' regime this day.