MicroMod WiFi Function Board - DA16200 Hookup Guide

≡ Pages
Contributors: Ell C

Software Installation

Note: This example assumes you are using the latest version of the Arduino IDE on your desktop. If this is your first time using Arduino, please review our tutorial on installing the Arduino IDE.

Arduino Board Definitions

We'll assume that you installed the necessary board files for your Processor Board. In this case, we used the MicroMod Artemis Processor Board.

MicroMod Artemis Processor Board Hookup Guide

October 21, 2020
Get started with the Artemis MicroMod Processor Board in this tutorial!

CH340 Driver

You may need to install CH340 driver for the USB-to-serial converter. Check out our section on "How to Install CH340 Drivers" for help with the installation.

Note: If applicable, make sure you are using the proper driver files for your CPU architecture. This is usually indicated by a folder or file name with "x86" for 32-bit processors or "x64" for 64-bit processors.

Main Board Example - Pin Connection Table

For the following examples, we are using the Artemis Processor Board. For DA16200 specific pins, here is the mapping to use in Arduino sketches:

AUDIO UART GPIO/BUS I2C SDIO SPI0 Dedicated
Function Board
Pin Name
I/O
Direction
Main Board's
Processor Pin
Slot 0 Slot 1
VCC Input -
3.3V Input -
GND - -
RTC_WAKE1 Input G2 G7
RTC_WAKE2 Output G1 G6
RTC_PWR_KEY Input G0 G5
GPIOA11 PWM0 PWM1
CS CS0 CS1
GPIOA10 D0 D1