MicroMod WiFi Function Board - DA16200 Hookup Guide

≡ Pages
Contributors: Ell C

Introduction

Want to add all the IoT functionality of the DA16200 to the adaptability of the MicroMod system? Then you're in luck! The SparkFun MicroMod DA16200 Function Board adds a fully integrated WiFi module with a 40MHz crystal oscillator, 32.768KHz RTC clock, RF Lumped RF filter, 4MB flash memory, and an on-board chip antenna to any MicroMod project. With the addition of JTAG connectors for deep dive programming, you've got everything you need to get your MicroMod setup ready for your next IoT project.

SparkFun MicroMod WiFi Function Board - DA16200

WRL-18594
Retired

Required Materials

To follow along with this tutorial, you will need the following materials at a minimum. You may not need everything though depending on what you have. Add it to your cart, read through the guide, and adjust the cart as necessary.

Reversible USB A to C Cable - 2m

CAB-15424
$10.50

SparkFun MicroMod Artemis Processor

DEV-16401
$17.50

SparkFun MicroMod Main Board - Single

DEV-18575
Retired

SparkFun MicroMod WiFi Function Board - DA16200

WRL-18594
Retired

MicroMod Main Board

To hold the processor board and function board, you will need one Main board. Depending on your application, you may choose to have one or two additional function boards.

SparkFun MicroMod Main Board - Single

DEV-18575
Retired

SparkFun MicroMod Main Board - Double

DEV-18576
Retired

MicroMod Processor Board

There are a variety of MicroMod Processor Boards available to choose from.

SparkFun MicroMod Artemis Processor

DEV-16401
$17.50

SparkFun MicroMod Teensy Processor

DEV-16402
$24.95

SparkFun MicroMod ESP32 Processor

WRL-16781
$19.95

SparkFun MicroMod mikroBUS Starter Kit

KIT-19935
$79.95 $59.95

Tools

You will need a screw driver to secure the Processor and Function boards.

SparkFun Mini Screwdriver

TOL-09146
$1.50

MicroMod Screwdriver

TOL-19012
$0.75

Suggested Reading

If you aren’t familiar with the following concepts, we recommend checking out these tutorials before continuing.

Getting Started with MicroMod

Dive into the world of MicroMod - a compact interface to connect a microcontroller to various peripherals via the M.2 Connector!

MicroMod Artemis Processor Board Hookup Guide

Get started with the Artemis MicroMod Processor Board in this tutorial!

Designing with MicroMod

This tutorial will walk you through the specs of the MicroMod processor and carrier board as well as the basics of incorporating the MicroMod form factor into your own PCB designs!