MicroMod WiFi Function Board - DA16200 Hookup Guide

≡ Pages
Contributors: Ell C

Hardware Overview

DA16200

The MicroMod WiFi Function Board includes the DA16200 module from Dialog with AT command firmware. This chip is a fully integrated Wi-FiĀ® module with ultra-low power consumption, 40 MHz crystal oscillator, 32.768 KHz RTC clock, RF Lumped RF filter, 4 M-byte flash memory, and an onboard chip antenna. For more information, refer to the datasheet.

Wifi module is highlighted

Power

To power the board, you will need to apply power to a SparkFun Main Board; either a Single or a Double. Power applied will connect to the Function Board's VIN pin, which will be regulated down for the rest of the board with the AP2112 3.3V/600mA voltage regulator.

USB C of the Main board with USBC cable plugged in is highlighted

AP2112

Operating voltage for the DA16200 is 3.3 V. The AP2112 can handle a voltage range of 2.5-6V with a 600mA output and ensures appropriate voltage to the WiFi unit.

Voltage regulator is highlighted

CH340

The board is populated with the CH340E USB-to-Serial converter to update firmware on the DA16200 through its USB Type C connector. You will need a Main Board and a second USB cable to update the firmware.

CH340 and USB C are highlighted on the function board

Reset Button

The reset button allows users to reset the program running on the Dialog module without unplugging the board.

Factory Reset Button is highlighted

WPS Button

The Wi-Fi Protected Setup Button allows you to easily and quickly connect to a WiFi network.

WPS Button is highlighted

EEPROM

The board includes an I2C EEPROM. To enable writing to the EEPROM, pull WP low, either through the EEPROM_WP pin or by closing JP3.

EEProm is highlighted

JTAG

An unpopulated JTAG footprint is available for more advanced users who need breakpoint level debugging. We recommend checking out our JTAG section for the compatible male header and a compatible JTAG programmer and debugger.

JTAG pins are highlighted

LED

There is only one LED available which is the Power LED. The LED lights up to indicate availability for the DA16200 from the 3.3V voltage regulator. You can disable it by cutting the jumper on the back of the board (see Jumpers below).

Power LED is just below the WiFi module on the right side of the board

Jumpers

The following jumpers are included to configure the board.

  • PWR - By default, the jumper with the label PWR is closed. This jumper connects the 3.3V line and LED. Cutting this jumper will disable the LED.

Power LED Jumper is on the back of the board on the opposite side from the M2 connector

  • I2C Pull-up Resistors - By default, this three way jumper labeled I2C is closed and connects two pull-up resistors to the I2C data lines. If you have many devices on your I2C data lines, then you may consider cutting these two jumpers.

I2C jumper is on the front of the board to the left of the WPS button

  • WP - By default, write protect for the EEPROM is on. To disable write protection, close this jumper.

Write protect jumper is on the back of the board just next to the M2 Connector

Hardware Pinout

The M.2 connector on the MicroMod WiFi Function Board - DA16200 is routed according to the pinout chart below:

Highlighted function board M.2 connector

Depending on your window size, you may need to use the horizontal scroll bar at the bottom of the table to view the additional pin functions. Note that the M.2 connector pins on opposing sides are offset from each other as indicated by the bottom pins where it says (Not Connected)*. There is no connection to pins that have a "-" under the primary function.

AUDIO UART GPIO/BUS I2C SDIO SPI0 Dedicated
Description Function Bottom
Pin
   Top   
Pin
Function Description
(Not Connected) 75 GND
- 74 73 3.3V Power Supply: 3.3-6V
- 72 71 Power EN Power Supply: 3.3-6V
- 70 69 -
- 66 65 -
- 64 63 -
- 62 61 -
- 60 59 -
- 58 57 RTC_WAKE1 This pin is an input pin for receiving an external event signal from an external device like a sensor. The RTC block detects an external event signal via this pin and wakes up DA16200 from Sleep mode 2 or Sleep mode 3.
- 56 55 RTC_WAKE2 This pin is an input pin for receiving an external event signal from an external device like a sensor. The RTC block detects an external event signal via this pin and wakes up DA16200 from Sleep mode 2 or Sleep mode 3.
- 54 53 RTC_PWR_KEY Enable to kick off a predefined power-up sequence and eventually all the necessary power is supplied to all the sub-blocks including the main digital block in DA16200. When disabled, all blocks are powered off and this mode is defined as Sleep mode 1.
- 52 51 GPIOA11
- 50 49 CS
- 48 47 GPIOA10
- 46 45 GND
- 44 43 -
- 42 41 -
Controls the write protection pin for the EEPROM. Pull low to enable. EEPROM_WP 40 39 GND
- 38 37 -
Controls EEPROM's I2C address configuration. EEPROM_A0 36 35 -
Controls EEPROM's I2C address configuration. EEPROM_A1 34 33 GND
Controls EEPROM's I2C address configuration. EEPROM_A2 32 31 Module Key
Module Key 30 29 Module Key
Module Key 28 27 Module Key
Module Key 26 25 Module Key
Module Key 24 23 -
- 22 21 I2C_SCL I2C - Clock signal for EEPROM
- 20 19 I2C_SDA I2C - Data signal for EEPROM
- 18 17 -
- 16 15 U1_RXI
- 14 13 U1_TXO
- 12 11 -
- 10 9 -
- 8 7 CIPO
- 6 5 COPI
- 4 3 SCK
- 2 1 GND

Board Dimensions

The board uses the standard MicroMod Function Board size which measures about 1.50"x2.56".

Board Dimensions