MicroMod WiFi Function Board - DA16200 Hookup Guide

≡ Pages
Contributors: Ell C

Hardware Hookup

Adding a Processor Board to the Main Board

Align the top key of the MicroMod Artemis Processor Board to the Processor screw terminal of your Main Board and angle the board into the socket. Insert the board at an angle into the M.2 connector.

Note: There is no way to insert the processor backward since the key prevents it from mating with the M.2 connector and as an extra safeguard to prevent inserting a processor that matches the key, the mounting screw is offset so you will not be able to secure an improperly connected processor board.

The Processor Board will stick up at an angle, as seen here:

Main board with Processor Board sticking up at an angle

Once the board is in the socket, gently push the MicroMod Processor Board down and tighten the screw with a Phillip's head.

Main board with Processor Board screwed in

Adding a Function Board to the Main Board

As with the Processor Board, align the top key of the MicroMod WiFi Function Board to the screw terminal of your Main Board on the Function Board side and angle the board into the socket. Insert the board at an angle into the M.2 connector.

Main board with Function Board sticking up at an angle

Once the board is in the socket, gently push the MicroMod Function Board down and tighten the screws with a Phillip's head.

Main board with Function Board screwed in

Once both boards are secure, your assembled MicroMod system should look similar to the image below!

Assembled main board with both processor and function boards securely fastened

DA16200 Firmware Update

To update the firmware you will need to connect the USB C cable to the MicroMod WiFi Function Board (DA16200) to a computer's COM port. An additional Main Board with a second USB C cable is also needed to power the Main Board and MicroMod WiFi Function Board.

USBC outlet on function board