micro:climate Kit Experiment Guide

≡ Pages
Contributors: bboyho, D___Run___

About the weather:bit

The weather:bit is a carrier board for the micro:bit. Similar to an Arduino shield, it is designed to add functionality to the micro:bit without the hassle of a number of other boards, components and all of those jumper wires.

SparkFun weather:bit - micro:bit Carrier Board (Qwiic)

DEV-15837
$17.95

In this case, the weather:bit takes your normal run-of-the-mill micro:bit and turns it into a full-blown weather station with a few extra parts, which you can use to measure the following:

  • Air Temperature
  • Relative Humidity
  • Barometric Pressure
  • Wind Speed
  • Wind Direction
  • Rain Fall
  • Soil Moisture
  • Soil Temperature

Phewwwww! That is a lot of data for such a tiny computer! Let's take a closer look at this board and check it out for ourselves.

Edge Connector

The weather:bit connects to the micro:bit via an edge pin connector. This makes it handy to swap out micro:bits for programming, but also gives reliable connections to all of the different pins on the micro:bit.

EdgeConnector

BME280 Barometric Pressure Sensor

The weather:bit has a BME280 barometric pressure sensor onboard, which can measure air temperature, humidity, barometric pressure and altitude. It communicates with the micro:bit via I2C, and the data from this sensor is easily accessible using the SparkFun weather:bit extension for MakeCode.

BME280

Weather Meter Sockets

There are two RJ11 jacks at the bottom of the weather:bit. These are used to connect our weather meters to the weather:bit.

RJ11 Wind Rain

These meters enable you to measure the wind speed and direction, as well as rain fall.

weather meter hooked u

Again, these are easily accessible in MakeCode via our SparkFun weather:bit extension.

Soil Moisture and Temperature

Between the two RJ11 jacks are two sets of screw terminals sets.

Soil Moisture and Temp Screw Terminals

The one on the left is used to hook up a soil moisture sensor. You can use either longer jumper wires or wires cut to whatever length works for your project.

Soil Moisture

The set on the right is the soil temperature sensor. It is set up to use our waterproof temperature sensor. This sensors wire is rather long and is great for monitoring the temperature of the soil in your garden so that you know the exact moment the ground is ready for planting those tomatoes!

Soil Temperature

Serial Port

We have populated the serial port pins with a standard FTDI format to make it easy for you to plug in a serial widget of your choice, such as an OpenLog or Serial LCD display, or to just monitor data through an FTDI breakout and USB cable.

Serial Port

I2C Port

For those of you who are more adventurous and demand a way to hook up other sensors of your choice, we have added an I2C port that can be soldered to directly --- or you can add headers for plug-and-play use of your I2C sensors and actuators.

I2C