LSM6DS3 Breakout Hookup Guide

≡ Pages
Contributors: MTaylor

Introduction

The LSM6DS3 is a accelerometer and gyroscope sensor with a giant 8 kbyte buffer and embedded processing interrupt functions, specifically targed at the cellphone market. The sensor is super-flexible and can be configured specifically for an application. We've put together a driver and slew of examples to help you explore the possibilities.

SparkFun 6 Degrees of Freedom Breakout - LSM6DS3

SEN-13339
Retired

Some of the things the LSM6DS3 can do:

  • Read accelerometer data up to 6.7 kilosamples per second, for super accurate movement sensing
  • Read gyroscope data up to 1.7 kilosamples per second
  • Operates at 1.25mA for up to 1.7 ksps modes
  • Read temperature
  • Buffer up to 8 kbytes of data between reads (built-in FIFO)
  • Count steps (Pedometer)
  • Detect shocks, tilt, motion, taps, double-taps
  • Host other sensors into its FIFO
  • Drive interrupt pins by embedded functions or by FIFO low-capacity/overflow warning.

Covered In This Tutorial

This tutorial gives you all you need to get going with the LSM6DS3. We'll introduce you to the chip itself, then the breakout board. Then we'll switch over to example code and show you how to interface with the board using an Arduino and our SparkFun LSM6DS3 Arduino library.

The tutorial is split into the following pages:

Required Materials

Get the datasheet and application notes now. Open them in a non-browser viewer that can display the index/table of contents in a pane. There is so much information, paned viewing is a must!

This tutorial explains how to use the LSM6DS3 Breakout Board with an Arduino. To follow along, you'll need the following materials:

The LSM6DS3 is a 3.3V device! Supplying voltages greater than ~3.6V can permanently damage the IC. As long as your Arduino has a 3.3V supply output, and you're OK with using I2C, you shouldn't need any extra level shifting. But if you want to use SPI, you may need a level shifter.

A logic level shifter is required for any 5V-operating Arduino (UNO, RedBoard, Leonardo, etc). If you use a 3.3V-based 'duino -- like the Arduino Pro 3.3V or 3.3V Pro Mini -- there is no need for level shifting.

Suggested Reading

If you're not familiar with some of the concepts below, we recommend checking out that tutorial before continuing on.