LilyPad ProtoSnap Plus Hookup Guide

≡ Pages
Contributors: MikeGrusin, Gella

Using the Expansion Ports

The LilyPad ProtoSnap Plus features five expansion ports connected to sew tabs on the LilyPad USB Plus. These allow you to easily attach external components to the board, including LilyPad and non-LilyPad boards. The expansion ports can accommodate alligator clips, IC clips, and other temporary attachment cables for testing and experimentation. Below are a few ways to connect an alligator cable to the sew tabs.

Alligator Clip Parallel to a Sew Tab

Alligator clip attached parallel to the expansion port.

Alligator Clip Perpendicular to a Sew Tab

Alligator clip attached perpenticular to the expansion port.

Testing a LilyPad Temperature Sensor

A LilyPad temperature sensor attached to the LilyPad ProtoSnap Plus expansion ports for testing.

Using Expansion Port A9

You may have noticed that tab A9 is connected to both the LilyPad Slide Switch and an Expansion Port. You can only use A9 for one of these connections; either the switch as an input or the expansion port as an input/output.

If you're using an external component or sensor on expansion port A9, move the slide switch to the OFF position to keep the switch from interfering with your input or output signal.

Turn Switch OFF for A9

Below is an image of the LilyPad temperature sensor attached to the LilyPad ProtoSnap Plus expansion ports for testing.

Testing Temperature Sensor

For more information about about expansion port A9 in the Technical Notes section.