Getting Started with the SmartLED Shield for Teensy

≡ Pages
Contributors: bboyho

Introduction

The PixelMatix SmartLED shield for Teensy makes it easy to connect to RGB LED matrix panels! The shield makes it easy to connect to the 16 pins required to drive the display, connects an external 5V supply to power the display and Teensy, and brings out the Teensy’s free signals to a convenient header.

SmartLED Shield V4 for Teensy 3

DEV-15046
Retired
Note: This tutorial was originally written for the SmartLED Shield V4 for Teensy 3. If you are using a Teensy 4, we recommend using the SmartLED Shield V5 or an adapter. Make sure to check out the compatibility notes for more information.

In this tutorial, we will explore a some of the examples provided with the SmartLED shield using different RGB LED matrix panel sizes.

SmartLED Demos with Different Panels

Required Materials

To follow along with this tutorial, you will need the following materials. You may not need everything though depending on what you have. Add it to your cart, read through the guide, and adjust the cart as necessary.

RGB LED Matrix Panel

You will need a panel. The following has been tested to work with the examples provided.

RGB LED Matrix Panel - 32x32

COM-14646
$48.50

RGB LED Matrix Panel - 32x64

COM-14718
Retired

RGB LED Matrix Panel - 64x64

COM-14824
Retired

Teensy

To control the panel using the SmartLED shield, you will need a Teensy. You can use a Teensy 4.0 but you would need to make sure that you are using the appropriate SmartLED Shield version or adapter.

Teensy 3.2

DEV-13736
Retired

Teensy 3.5

DEV-14055
Retired

Teensy 3.5 (Headers)

DEV-14056
Retired

Teensy 3.6

DEV-14057
Retired

Teensy 3.6 (Headers)

DEV-14058
Retired

Power

You will also need a 5V power supply. A 5V wall adapter and barrel jack adapter is the easiest way to connect power to the panel and Teensy. However, there are other methods depending on how you are powering the panel.

DC Barrel Jack Adapter - Female

PRT-10288
$3.75

Wall Adapter Power Supply - 5VDC, 2A (Barrel Jack)

TOL-15312
$9.50

Additional Components

Depending on your setup and how you are controlling the panel, you may need these additional components.

Straight Header - Male (PTH, 0.1in., 40-Pin)

PRT-00116
$1.95

USB Micro-B Cable - 6 Foot

CAB-10215
$6.50

Right Angle Header - Male (PTH, 0.1in., 40-Pin)

PRT-00553
$2.50

SparkFun Real Time Clock Module

BOB-12708
$8.50

microSD USB Reader

COM-13004
Retired

microSD Card - 16GB (Class 10)

COM-15051
Retired

Tools

Depending on your setup, you may need pliers, a soldering iron, solder, and general soldering accessories.

Solder Lead Free - 100-gram Spool

TOL-09325
$24.95

Needle Nose Pliers

TOL-08793
$3.60

SparkFun Mini Screwdriver

TOL-09146
$1.50

Weller WLC100 Soldering Station

TOL-14228
Retired

Suggested Reading

If you aren’t familiar with the following concepts, we recommend checking out these tutorials before continuing.

How to Power a Project

A tutorial to help figure out the power requirements of your project.

What is an Arduino?

What is this 'Arduino' thing anyway? This tutorials dives into what an Arduino is and along with Arduino projects and widgets.

RGB Panel Hookup Guide

Make bright, colorful displays using the 32x16, 32x32, and 32x64 RGB LED matrix panels. This hookup guide shows how to hook up these panels and control them with an Arduino.

Getting Started with the Teensy

Basic intro to the Teensy line of products, with soldering and programming suggestions.