Getting Started with the Raspberry Pi Zero 2 W

≡ Pages
Contributors: M-Short, El Duderino

Resources and Going Further

At this point your Pi Zero 2 W should be acting similar to any other computer. From here, you can teach yourself the finer points of Linux, learn Python, program the GPIO pins, setup a Minecraft™ server, build a network storage system, game console, or media center, or just surf the web.

For more information about the Pi Zero 2 W or Raspberry Pi in general, check out these resources:

Looking to make the Raspberry Pi Zero W a dongle? Check out the Pi Zero USB Stem:

Need some inspiration? Check out these tutorials and projects.

FLIR Lepton Hookup Guide

See the invisible world of infrared radiation using the FLIR Dev Kit and Raspberry Pi.

Basic Servo Control for Beginners

An introductory tutorial demonstrating several ways to use and interact with servo motors!

Pro Micro RP2040 Hookup Guide

This tutorial covers the basic functionality of the Pro Micro RP2040 and highlights the features of the dual-core ARM Cortex-M0+ processors development board. Get started with the first microcontroller from the Raspberry Pi Foundation!

Qwiic Kit for Raspberry Pi V2 Hookup Guide

Get started with the SGP40, BME280, VCNL4040, and microOLED via I2C using the Qwiic system and Python on a Raspberry Pi! Measure VOC Index, light, temperature, humidity, and pressure from the environment. Then display them on the microOLED, serial terminal, or the cloud with Cayenne!