AVR-Based Serial Enabled LCDs Hookup Guide

≡ Pages
Contributors: QCPete

Serial UART: Example Code - Basic

You can download the latest example code for this experiment from the GitHub repo or you can copy and paste the following code into your Arduino IDE:

language:cpp
/*
 OpenLCD is an LCD with serial/I2C/SPI interfaces.
 By: Nathan Seidle
 SparkFun Electronics
 Date: April 19th, 2015
 License: This code is public domain but you buy me a beer if you use this and we meet someday (Beerware license).

 This example shows how to display a counter on the display over serial. We use software serial because if 
 OpenLCD is attached to an Arduino's hardware serial port during bootloading  it can cause problems for both devices.

 To get this code to work, attached an OpenLCD to an Arduino Uno using the following pins:
 RX (OpenLCD) to Pin 7 (Arduino)
 VIN to 5V
 GND to GND

*/

#include <SoftwareSerial.h>

SoftwareSerial OpenLCD(6, 7); //RX, TX

byte counter = 0;
byte contrast = 2; //Lower is more contrast. 0 to 5 works for most displays.

void setup()
{
  Serial.begin(9600); //Start serial communication at 9600 for debug statements
  Serial.println("OpenLCD Example Code");

  OpenLCD.begin(9600); //Start communication with OpenLCD

  //Send contrast setting
  OpenLCD.write('|'); //Put LCD into setting mode
  OpenLCD.write(24); //Send contrast command
  OpenLCD.write(contrast);

}

void loop()
{
  //Send the clear command to the display - this returns the cursor to the beginning of the display
  OpenLCD.write('|'); //Setting character
  OpenLCD.write('-'); //Clear display

  OpenLCD.print("Hello World!    Counter: "); //For 16x2 LCD
  //OpenLCD.print("Hello World!        Counter: "); //For 20x4 LCD
  OpenLCD.print(counter++);

  delay(250); //Hang out for a bit
}

Here's what you should see after uploading the code to your Arduino. Try changing the text with a different message!

Hello World! Counter: 11 is displayed on LCD screen once code is uploaded to the redboard

To send text to the board, wait 1/2 second (500ms) after power up for the splash screen to clear, then send text to the display through your serial port. The display understands all of the standard ASCII characters (upper and lowercase text, numbers, and punctuation), plus a number of graphic symbols and Japanese characters. See the HD44780 datasheet for the full list of supported characters.

If you send data that goes past the end of the first line, it will skip to the start of the second line. If you go past the end of the second line, the display will jump back up to the beginning of the first line.