TeensyView Hookup Guide

≡ Pages
Contributors: MTaylor

Resources and Going Further

The TeensyView was designed to be as flexible as possible while still being able to nest down into a low-profile addition to the Teensy.

alt text

Some various TeensyView-Teensy connections. The bottom centermost TeensyView was created using this guide, while the left is a minimal non-separable configuration. Using a breadboard is also an option.

The TeensyView works with some really heavy examples, but they're really only demonstrations. What to do with it is up to you! They're great for adding simple debug info to a mobile project, while a diligent pixel artist could implement a whole menu system.

More information about the SSD1306 controller and the TeensyView design can be found here:

Additional projects and sketches that use the TeensyView:

  • The HighSpeedTest, in the examples folder, draws alternating pixels as fast as possible. This can be used to experiment with the limits of the TeensyView's OLED.

For additional inspiration, check out these other tutorials based on displays:

ELasto-Nightlight

Fear the dark no longer with this ELastoLite nightlight.

FemtoBuck Constant Current LED Driver Hookup Guide v13

The FemtoBuck board is a high-efficiency, single-channel constant-current LED driver.

SparkFun Qwiic Alphanumeric Display Hookup Guide

A Hookup Guide to get you started with the Qwiic Alphanumeric Display.

Turn a Qwiic Ultrasonic Distance Sensor into a Garage Distance Sensor

This tutorial will take your SparkFun Qwiic Ultrasonic Distance Sensor to the next level by turning it into a parking distance sensor!