SparkFun Auto pHAT Hookup Guide

≡ Pages
Contributors: santaimpersonator

Hardware Overview

Below, is an overview of the major hardware components on the Auto pHAT.

Dimensions

The overall dimensions of the Auto pHAT are 57mm x 65mm. For more details, users can check out the layout in the Eagle files. The board also features two cut-outs for the camera and display ribbon connections.

Dimensions
Dimensions of the Auto pHAT. (Click to enlarge)

GPIO Connections

As the Auto pHAT is also intended to integrate with other HATs, it is important to know all of the pin being utilized to avoid conflicts. Below is a layout of all the GPIO pins being utilized by the hardware on the Auto pHAT. (*Click the following links, for more information on the GPIO mapping of the Raspberry Pi or Jetson Nano.)

GPIO Top
GPIO header connection on the top of the Auto pHAT.
GPIO Bottom
GPIO header connection on the bottom of the Auto pHAT.
(Click to enlarge)

Raspberry Pi GPIO Map

GPIO Pins Standard GPIO layout on the Raspberry Pi.
Image courtesy of the Raspberry Pi Foundation.

Power Connections

Power to the Auto pHAT is supplied through the GPIO pins; both 5V and 3.3V are utilized.

Pin # GPIO
1 3.3V
17 3.3V
2 5V
4 5V
6 GND
9 GND
Pin # GPIO
14 GND
20 GND
30 GND
34 GND
39 GND

Qwiic (I2C)

IMU (I2C)
Pin # GPIO Function
3 GPIO 02 (SDA) Qwiic (SDA)
5 GPIO 03 (SCL) Qwiic (SCL)
26 GPIO 7 Interrupt


Encoder (I2C)
Pin # GPIO Function
3 GPIO 02 (SDA) Qwiic (SDA)
5 GPIO 03 (SCL) Qwiic (SCL)
7 GPIO 4 Interrupt
Motor Driver (I2C)
Pin # GPIO Function
3 GPIO 02 (SDA) Qwiic (SDA)
5 GPIO 03 (SCL) Qwiic (SCL)
Servo Controller (I2C)
Pin # GPIO Function
3 GPIO 02 (SDA) Qwiic (SDA)
5 GPIO 03 (SCL) Qwiic (SCL)
Qwiic Connector
Pin # GPIO Function
3 GPIO 02 (SDA) Qwiic (SDA)
5 GPIO 03 (SCL) Qwiic (SCL)

Servo Controller

The servo controller utilizes the same PCA9685 IC used on the Pi Servo pHAT; however, only the first 4 PWM channels are broken out. The PCA9685 provides I2C control over the 16-channels of 12-bit pulse width modulation (PWM); although only the first 4-channels are available on the Auto pHAT. The default I2C address for the servo controller on the Auto pHAT is 0x40.

PCA9685
The PCA9685 16-channel PWM controller IC and output headers.

Characteristic Description
Operating Voltage (VDD) 2.3 V to 5.5 V (Hardwired: 5V)
Operating Temperature -40°C to 85°C
PWM Outputs 16 Totem pole outputs (Default: Open-Drain)
Sink 25 mA or Source 10 mA (at 5V)
Shared PWM frequency
Supports hot insertion
PWM Frequency 24Hz to 1526 Hz (Default (1Eh): 200Hz)
PWM Resolution 12-bit (4096 steps of control)
Duty Cycle 0% to 100% (adjustable)
Oscillator Internal: 25 MHz (Hardwired)
External: 50 MHz (max.) input (unavailable)
I2C Address 8 available hardware configurable addresses
  • Configuration Jumpers: 0x40 to 0x47
  • Default: 0x40
4 programmable addresses to allow simultaneous groups control of multiple devices:
  • 1- General All Call address.
  • 3- Sub Call addresses.
Note: For more details on the PCA9685 and its utilization as a servo controller, check out the following hookup guides on the Pi Servo pHATs:

Pi Servo Hat Hookup Guide

September 14, 2017
This hookup guide will show you how to connect and use the Pi Servo Hat in a project.

Pi Servo pHAT (v2) Hookup Guide

July 11, 2019
This hookup guide will get you started with connecting and using the Pi Servo pHAT on a Raspberry Pi.

Motor Driver

The motor driver consists of the same PSoC4245 and DRV8835 as the Serial Controlled Motor Driver and Qwiic Motor Driver. The DRV8835 H-Bridge provides two drive outputs, each capable of 1.2A at steady state. The default I2C address for the motor driver on the Auto pHAT is 0x5D.

PSoc4245 and DRV8835
The PSoc4245 microcontroller, DRV8835 H-Bridge, and screw terminal outputs.

Characteristic Description
Operating Voltage (VDD) 3 V to 11 V (Hardwired: 5V)
Drive Channels 2 Channels
Drive Strength 1.5A per channel (max.)
1.2A (steady state)
Drive Control 127 levels of control
Direction inversion on a per motor basis
Global Drive enable
I2C Address 10 available hardware configurable addresses
  • Configuration Jumpers: 0x58 to 0x61
  • Default: 0x5D

Thermal Management

An important consideration for the motor driver is the thermal load due to the current draw of the motors. In order to dissipate the heat, users can use our Theragrip Thermal Tape to attach Small Heat Sinks across the thermally conductive area on the bottom of the board. As the thermal plane doesn't promote natural convection well, users can add a fan to help dissipate the energy, as well.

Thermally conductive area
Thermally conductive area on the bottom of the Auto pHAT.
Temp to Current Load Curve
Temperature to total driver load curve.
(Click to enlarge)

Note: For more details on the Serial Controller Motor Driver or Qwiic Motor Driver and its utilization, check out the following hookup guides on the Pi Servo pHATs:

Serial Controlled Motor Driver Hookup Guide

November 17, 2016
Hookup guide for the Serial Controlled Motor Driver

Hookup Guide for the Qwiic Motor Driver

September 19, 2019
Drive things "qwiic"-ly with the SparkFun Qwiic Motor Driver!

Encoder Reader

At the heart of the encoder reader is an ATtiny84, which is utilized on our pseudo I2C devices. The encoder reader is based off of the Qwiic Twist, but is capable of reading two, separate quadrature encoders. The default I2C address for the servo controller on the Auto pHAT is 0x73.

ATtiny84 encoder reader
The ATtiny84 dual encoder reader and screw terminal inputs.

9-DoF IMU

The 9-DoF (degree of freedom) IMU is the same ICM20948 IC used on the 9DoF IMU Breakout. It provides 10 unique measurements: 3 axes of acceleration, rotational rate, and magnetic strength data, as well as, internal temperature. Users should note the location of the IMU and the orientation of the axes (labeled on the board), when taking measurements. The default I2C address for the IMU on the Auto pHAT is 0x69.

ICM20948
The ICM20948 9-DoF IMU.

Characteristic Description
Operating Voltage (VDD) 1.71 V to 3.6 V (Hardwired: 1.8V)
Operating Temperature -40°C to 85°C
Gyroscope
Full Scale Ranges:
  • ±250 dps
  • ±500 dps
  • ±1000 dps
  • ±2000 dps
Sensitivity:
  • ±(1/131) dps
  • ±(1/65.5) dps
  • ±(1/32.8) dps
  • ±(1/16.4) dps
Output Data Rate: 562.5, 1125, 9000 Hz
Accelerometer
Full Scale Ranges:
  • ±2 G
  • ±4 G
  • ±8 G
  • ±16 G
Sensitivity:
  • ±(1/16384) G
  • ±(1/8192) G<
  • ±(1/4096) G<
  • ±(1/2048) G<
Output Data Rate: 562.5, 1125, 4500 Hz
Magnetometer Full Scale Range: ±4900 µT
Sensitivity: .15 µT
Output Data Rate: 100 Hz
I2C Address 2 hardware configurable addresses:
  • 0x69: Jumper closed (Default)
  • 0x68: Jumper open

Note: For more details on the ICM-20948 and its utilization as an IMU, check out the following hookup guide:

SparkFun 9DoF IMU (ICM-20948) Breakout Hookup Guide

June 27, 2019
How to use the SparkFun 9DoF ICM-20948 breakout board for your motion sensing projects. This breakout is ideal for wearable sensors and IoT applications.

Qwiic Connector

A connector is provided for attaching other Qwiic devices.

Auto pHAT Qwiic Connector
Qwiic connector.

Note: While most of our Qwiic devices should be compatible with a single board computer (SBC), not all have a supported Python package. Users who are unfamiliar with our Qwiic connect system, can check out the video below: