RedBot Assembly Guide Rev 02

This Tutorial is Retired!

This tutorial covers concepts or technologies that are no longer current. It's still here for you to read and enjoy, but may not be as useful as our newest tutorials.

≡ Pages
Contributors: HelloTechie, SFUptownMaker

RedBot Mainboard

In this section, you will adding the brains of the robot: the RedBot Mainboard.

Locate the Following:

4x 4-40 x 1/4" Phillips Screw 1x RedBot Mainboard
4-40 x 1/4 inch Phillips Screw RedBot Mainboard

Adding the RedBot Mainboard

Line up the four corner holes of the RedBot Mainboard to the four 4-40 x ⅜" metal standoffs on the top chassis piece. You will want the barrel jack on the RedBot Mainboard to be on the left side. Using four 4-40 x 1/4" Phillips screws, tighten down the RedBot Mainboard to the four 4-40 x ⅜" metal standoffs.

RedBoard Mainboard