QuickLogic Thing Plus (EOS S3) Hookup Guide

≡ Pages
Contributors: bboyho

Introduction

This guide provides users with functional descriptions, configuration options for the QuickLogic Thing Plus EOS S3. It also serves as a “Getting Started” and “How To” guide.

SparkFun QuickLogic Thing Plus - EOS S3

DEV-17273
Retired

Required Materials

To follow along with this tutorial, you will need the following materials. You may not need everything though depending on what you have. Add it to your cart, read through the guide, and adjust the cart as necessary.

Reversible USB A to C Cable - 0.8m

CAB-15425
$6.50

SparkFun QuickLogic Thing Plus - EOS S3

DEV-17273
Retired

You Will Also Need

You will also need a computer with a terminal program or any UART console application. For the scope of this tutorial, we will use PuTTY.

  • Computer with Windows 10 OS or Linux OS
    • Serial Terminal

Suggested Reading

If you aren't familiar with the Qwiic system, we recommend reading here for an overview .

Qwiic Connect System
Qwiic Connect System

If you aren’t familiar with the following concepts, we also recommend checking out a few of these tutorials before continuing.

Serial Peripheral Interface (SPI)

SPI is commonly used to connect microcontrollers to peripherals such as sensors, shift registers, and SD cards.

Logic Levels

Learn the difference between 3.3V and 5V devices and logic levels.

Accelerometer Basics

A quick introduction to accelerometers, how they work, and why they're used.

I2C

An introduction to I2C, one of the main embedded communications protocols in use today.

Serial Terminal Basics

This tutorial will show you how to communicate with your serial devices using a variety of terminal emulator applications.