Proto Pedal Example: Analog Equalizer Project

≡ Pages
Contributors: Byron J.

Assembly

Step Zero

To begin, we'll assume that you've completed the basic assembly of the proto pedal board.

alt text

If you're using the Proto Pedal Chassis, you'll need to prepare it by drilling holes for two potentiometers, as shown in the Chassis Hookup Guide.

With the prerequisites complete, you can start the sequence below. We're going to be stepping in fairly large chunks. Each step lists the required components, so you can prepare them before you commence. Once they have been placed, double-check your solder joints, and compare your work to the photos.

Playing Battleship

In the following steps, we're going to use the grid notation seen on a standard solderless breadboard. From left to right, the columns are numbered 1 to 30, and, from bottom to top, the rows are assigned letters from A through J. Any hole in the center of the board can be referenced by number-letter coordinate, such as 27L or 7G.

alt text

Coordinates and rails.

Additionally, we'll be using the power and center rails of the proto area. At the top and bottom edge of the board are 9V power (AKA Vcc) on the traces marked + and ground on the traces marked -. One of the center traces is used as a half-rail bias voltage, which we'll refer to as Vref.

In the following steps, we'll give the coordinate designation of each component.

Step One: Wire Jumpers

The first step is to use solid core hookup wire, and make some basic connections between sets of pads in the proto area. For clarity, we're using many different colors of wire, but not using any red wire.

Jumper NumberColorStart CoordinateEnd Coordinate
1BlackIn1A
2Yellow2ALower Vcc
3Blue3E3F
4Green10JUpper Ground
5Yellow11JPot3 Left
6Black12JPot3 Right
7Blue17JPot3 Middle
8White18EPot4 Middle
9Green20JUpper Ground
10Bare11D12D
11Yellow12CVref
12Yellow13ALower Vcc
13Black16FOut
14Bare22G23G
15Bare21D22D
16Yellow23ALower Vcc

Installed, these jumpers look like this.

alt text

Jumper placement (click to enlarge).

The jumpers are soldered to the back of the board and trimmed close to the board. If the tails stick out too far, they will short to the metal enclosure.

alt text

When you're done, count the number of jumpers -- there should be sixteen in total. If you find that you're short, doublecheck that you've got the 0.1 inch wire links as noted in the photo.

Step Two: Resistors

There are eleven resistors in this design. To get started, select the following from your resistor assortment. We include the color markings below. The packaging of the resistor assortment serves as an illustrated guide.

Resistor ValueValue Color CodeStart CoordinateEnd CoordinatePlacement Notes
1M Ωbrown-black-green-gold1DVref
10K Ωbrown-black-orange-gold3BLower Ground
10K Ωbrown-black-orange-gold4G11G0.7" long
10K Ωbrown-black-orange-gold12H16H0.4" long
100K Ωbrown-black-yellow-gold10ALower Vcc
100K Ωbrown-black-yellow-gold10BLower GroundAt angle
47 Ωyellow-violet-black-gold13G16G
2.2K Ωred-red-red-gold21J24J
2.2K Ωred-red-red-gold24HVref
2.2K Ωred-red-red-gold26DVref
2.2K Ωred-red-red-gold20C26C0.6" long

These resistors get installed as shown below. Take note of a couple placement details: some of the resistors are stretched longer than you might expect, and one of the 100K Ω resistors is at an angle.

alt text

Resistor placement (click to enlarge).

Step Three: Capacitors

There are ten capacitors, as follows. The values are printed on the caps, and there is a value decoder on the package. The ceramic caps are the small yellow ones, and the electrolytic caps are small black cylinders.

Capacitor ValueValue MarkingStart CoordinateEnd CoordinateOrientation Notes
100 pf ceramic10112I16I
0.01 uf ceramic10318A20A
0.1 uf ceramic104Input Coupling
0.1 uf ceramic10422B24B
0.1 uf ceramic10424A26A
1 uf electrolytic1uf/50V17G19G`-` to right
1 uf electrolytic1uf/50V22I24I`-` to left
1 uf electrolytic1uf/50V19I21I`-` to left
10 uf electrolytic10uf/25VOutput Coupling`-` to right
10 uf electrolytic10uf/25V3H4H`-` to right

These capacitors are installed as shown below. We've noted the polarity orientation of the electrolytic caps above, also -- the body of the cap has a white stripe with "-" symbols printed to mark the negative leg.

alt text

Capacitor placement (click to enlarge).

Step Four: Semiconductors

There are two types of semiconductor devices used in this project. The MOSFET is part of the Discrete Semiconductor Kit.

ComponentMarkingStart CoordinateEnd CoordinateOrientation Notes
5LN01SP MOSFETYB3C1CPin1 in column 3
YB facing upwards
rounded edges facing downwards
DIP-8 IC Socket
for LM358
Row 10Row 13Spanning center trough
Notch facing right
DIP-8 IC Socket
for LM358
Row 20Row 23Spanning center trough
Notch facing right

alt text

Semiconduictor placement (click to enlarge).

Step Five: Flying Wires & Pots

This last step involves adding the pots to the board. We'll make a little subassembly out of them, then solder that to the PCB.

Because it needs to flex a bit, we're using stranded wire for this step. Cut the following pieces

Length (Inches)Lentgh (Metric)Color
2.5"5cmBlue
2.5"5cmRed
2.5"5cmBlue
5"13cmRed
5"13cmYellow
5"13cmGreen

First, orient the pots so the legs are facing the same direction. If you're using the enclosure, you can put the pots in the chassis holes to hold them in place while you work.

alt text

Use the shorter pieces of red wire to jump from pin 1 of the first pot to pin 1 of the second pot. Before soldering tie the longer piece of red wire to pin 1 of the first pot. Then, repeat the above, bridging from pin 3 to pin 3 with blue wire.

Next, solder the yellow wire to pin 2 of the first pot, and green wire to pin 2 of the other pot. The pot with the yellow wire is the low frequency control, and the pot with the green wire is the high frequency control.

alt text

At this point, you'll have four wires trailing from the subassembly. They meet the PCB as shown below, in the pot 3 and 4 areas.

alt text

Last Step: Insert the ICs

With the above steps completed, you can insert the IC's in the sockets, taking care to align the pin-1 marks. The dimple should be at the top-right corner, and the notch should be facing right. The legs come splayed out a little bit wider than the sockets -- they'll need to be bent in a little bit to fit.

alt text

IC Orientation (click to enlarge).

Now we can move on to testing the pedal!