Mini GPS Shield Hookup Guide

≡ Pages
Contributors: Alex the Giant

Resources and Going Further

For more information about the Mini GPS Shield, check out the links below:

Going Further

Now that you've got the Mini GPS Shield up and running, what project are you going to use this shield for? Need a little inspiration? Check out some of these tutorials!

  • GPS Wall Clock -- This project uses a GPS module to create a wall clock that you never need to set!
  • GPS Differential Vector Pointer -- In this tutorial you’ll learn how to use GPS receivers to have two objects, a base and a target, point towards one another. This can be used to aim sensors, antennas, lasers, etc. from one object to another over long distances.

Three Quick Tips About Using U.FL

Quick tips regarding how to connect, protect, and disconnect U.FL connectors.

GPS Geo-Mapping at the Push of a Button

Let's ramp up our GPS tracking skills with KML files and Google Earth. We'll make a tracker that logs location and allows us to visualize our steps with Google Earth.

SparkFun GPS Dead Reckoning NEO-M8U Hookup Guide

The u-blox NEO-M8U is a powerful GPS units that takes advantage of untethered dead reckoning (UDR) technology for navigation. The module provides continuous positioning for vehicles in urban environments and during complete signal loss (e.g. short tunnels and parking garages). We will quickly get you set up using the Qwiic ecosystem and Arduino so that you can start reading the output!

Getting Started with u-blox Thingstream and PointPerfect

Interested in high precision GNSS without setting up a base station?