MicroPython Programming Tutorial: Getting Started with the ESP32 Thing

≡ Pages
Contributors: Shawn Hymel

Setup

Serial Terminal Program

To communicate with the Read–Eval–Print Loop (REPL) running on the ESP32, you will need to install a serial terminal program for your particular operating system (OS). The following tutorial makes several good recommendations as to which programs to use for the 3 major operating systems:

Serial Terminal Basics

September 9, 2013
This tutorial will show you how to communicate with your serial devices using a variety of terminal emulator applications.

Text Editor

At the time of this writing, no major integrated development environments (IDEs) support MicroPython for the ESP32 (for example, Mu was developed for MicroPython but does not support the ESP32). As a result, you will need to write code in a raw text editor and then save the files as somename.py. Some recommended text editors that work well for writing code include:

Load MicroPython on the ESP32 Thing

Unfortunately, the ESP32 Thing does not come ready to run MicroPython programs out of the box. To run MicroPython on the ESP32, you will need to first load the interpreter on it. To do that, follow the steps outlined in the How to Load MicroPython on a Microcontroller Board (specifically, the steps found in the ESP32 Thing section).

How to Load MicroPython on a Microcontroller Board

September 4, 2018
This tutorial will show you how to load the MicroPython interpreter onto a variety of development boards.

Install Python on Your Computer

In order to upload MicroPython programs to the ESP32, we will use a tool called ampy, which is a Python script that can read and write files to a MicroPython board over a serial connection. Because ampy is a Python script that runs on a host computer, we will need to install Python.

Instructions for installing Python can be found at python.org. Download and run the installer for your OS, or use your OS's package manager to install Python (if you are on Linux). Ampy will run with Python 2 or Python 3, so choose whichever version you like (we recommend Python 3, as MicroPython is based on Python 3, so the language will be similar).

If you are installing on Windows, make sure the "Add Python <x.x> to PATH" checkbox is selected.

Add Python to PATH Checkbox

For more information on using Python on windows, see this link.

Install ampy

Once you have installed Python, open a terminal for your host computer, and enter the following command:

language:shell
pip install adafruit-ampy

You should see a printout showing that ampy was downloaded and installed.

Installing ampy