MicroPython Programming Tutorial: Getting Started with the ESP32 Thing

≡ Pages
Contributors: Shawn Hymel

Experiment 5: WiFi

While the possibilities of interacting with hardware directly connected to the ESP32 are endless, some real fun can be had connecting to the Internet. By being able to send and receive data to servers across the Internet, the ESP32 can download current weather or time data, upload sensor data, and respond to events (e.g. on Twitter) in real time. This is just the beginning of exploring the Internet of Things (IoT).

To demonstrate accessing the Internet, we will write a quick MicroPython program that connects to a local WiFi and downloads the example.com web page using an HTTP GET command.

Note: You will need a WiFi access point with connection to the Internet for this exercise.

Hardware Connections

We'll keep it simple this time--just the ESP32 Thing will be needed. We're going to use its built-in WiFi radio, get a web page, and then send the downloaded HTML contents over the serial connection.

ESP32 Thing by itself

Code: GET Some

In a new file, enter the following code (change <YOUR WIFI SSID> to the name of your WiFi network name and <YOUR WIFI PASSWORD> to the name of your WiFi's password--note that the name and password should be in quotation marks ""):

language:python
import machine
import sys
import network
import utime
import urequests

# Pin definitions
repl_button = machine.Pin(0, machine.Pin.IN, machine.Pin.PULL_UP)
repl_led = machine.Pin(5, machine.Pin.OUT)

# Network settings
wifi_ssid = "<YOUR WIFI SSID>"
wifi_password = "<YOUR WIFI PASSWORD>"

# Web page (non-SSL) to get
url = "http://example.com"

# Create a station object to store our connection
station = network.WLAN(network.STA_IF)
station.active(True)

# Continually try to connect to WiFi access point
while not station.isconnected():

    # Try to connect to WiFi access point
    print("Connecting...")
    station.connect(wifi_ssid, wifi_password)

    # Check to see if our REPL button is pressed over 10 seconds
    for i in range(100):
        if repl_button.value() == 0:
            print("Dropping to REPL")
            repl_led.value(1)
            sys.exit()
        utime.sleep_ms(100)

# Continually print out HTML from web page as long as we have a connection
while station.isconnected():

    # Display connection details
    print("Connected!")
    print("My IP Address:", station.ifconfig()[0])

    # Perform HTTP GET request on a non-SSL web
    response = urequests.get(url)

    # Display the contents of the page
    print(response.text)

    # Check to see if our REPL button is pressed over 10 seconds
    for i in range(100):
        if repl_button.value() == 0:
            print("Dropping to REPL")
            repl_led.value(1)
            sys.exit()
        utime.sleep_ms(100)

# If we lose connection, repeat this main.py and retry for a connection
print("Connection lost. Trying again.")

Save the file with a name like wifi.py. In a command terminal, navigate to the directory where wifi.py is stored. Hold down button 0 on the ESP32 Thing to exit its currently running program. Back in the command terminal, enter the following commands (<PORT> should be changed to your serial port name/location):

language:shell
cp wifi.py main.py
ampy --port <PORT> put main.py

Open a serial connection to the ESP32, and you should see your ESP32 connect to your WiFi network and then download the example.com HTML page. If you see text like the one below, you know that it worked:

Printing HTML to the terminal from the ESP32

If you are unable to connect and download the page, double-check the SSID and password in the code. Additionally, some network configurations do not work well with the ESP32, which means you might need to try a different network.

Code to Note

In this example, we're relying on the network and urequests modules to handle much of the networking for us. We use the network module to perform the low-level communication over WiFi, including connecting to our Wifi access point. To create a connection to our WiFi access point, we first create a WLAN object and use network.STA_IF to tell the ESP32 that we want to use it as a client that connects to a separate access point:

language:python
station = network.WLAN(network.STA_IF)
station.active(True)

From there, we attempt to establish a connection with the access point:

language:python
while not station.isconnected():

    # Try to connect to WiFi access point
    print("Connecting...")
    station.connect(wifi_ssid, wifi_password)

The line station.connect(wifi_ssid, wifi_password) is what actually performs the connection. We wrap this up in a while loop that continually checks to see if we have a connection. This way, if no connection is established, the program will not move forward and try to perform a GET request on a website. Notice that we also include our "Drop to REPL" button check in this while loop, too, in case the ESP32 gets stuck here.

Once we have a connection, we use the urequests module to perform our GET request on example.com:

language:python
response = urequests.get(url)

This returns a Response object that contains all the information returned by the server. We can view the response in text form with the command:

language:python
print(response.text)

We then wait for 10 seconds before requesting the page again. During those 10 seconds, we check for a button 0 push every 100 ms.

If you would like to learn more about networking in MicroPython, see the network module documentation.