MicroMod Alorium Sno M2 Processor Board Hookup Guide
Contributors:
Member #798807, Ell C
Resources and Going Further
For more information, check out the resources below:
- Schematic
- Eagle Files
- Board Outline
- Alorium Technology OEM Module page
- Snō Product Brief
- GitHub Repo
For more information about the SparkFun MicroMod Ecosystem, take a look at the links below:
Need some inspiration for a project using your Alorium Sno Processor? The tutorials below may help you get started!
Designing with MicroMod
This tutorial will walk you through the specs of the MicroMod processor and carrier board as well as the basics of incorporating the MicroMod form factor into your own PCB designs!
MicroMod Update Tool Hookup Guide
Follow this guide to learn how to use the MicroMod Update Tool to interact directly with the UART on the MicroMod Asset Tracker's SARA-R5. Using this board you can talk directly to the module using u-blox's m-center software as well as update the firmware using EasyFlash.
MicroMod Main Board Hookup Guide
The MicroMod Main Board - Single and Double are specialized carrier boards that allow you to interface a Processor Board with a Function Board(s). The modular system allows you to add an additional feature(s) to a Processor Board with the help of a Function Board(s). In this tutorial, we will focus on the basic functionality of the Main Board - Single and Main Board - Double.