MicroMod Alorium Sno M2 Processor Board Hookup Guide

≡ Pages
Contributors: Member #798807, Ell C

Hardware Overview

M.2 Connector

All of our MicroMod Processor Boards come equipped with the M.2 MicroMod Connector, which leverages the M.2 standard and specification to allow you to install your MicroMod Processor Board on your choice of carrier board. Most of the pins use a common pinout to ensure cross platform compatibility.

M.2 Edge Connector Pins Highlighted

Alorium Technology Sno M2 Processor

The Alorium Technology Sno FPGA provides a reconfigurable hardware platform that hosts an ATmega328 instruction set compatible microcontroller. The FPGA also provides the ability to implement custom logic that accelerates specific functionality that is slow, problematic or even impossible for an 8-bit microcontroller.

The Alorium Sno Processor is the giant chip in the middle of the board

JTAG

The JTAG interface on Sno M2 is primarily used during manufacturing to load the production FPGA image. For advanced users, JTAG can be used for creating bare-metal FPGA designs and directly flashing a new image to the FPGA.

JTAG is highlighted on the upper left corner of the MicroMod board, with the M.2 connectors facing down.

FTDI

The FTDI facilitates USB communication - drivers for the FTDI chip may need to be installed. Please see the How to Install FTDI drivers tutorial if you need help installing these drivers.

FTDI chip is highlighted - it is the small square chip on the lower right side of the front of the board when the M2 connector is pointing down

LEDs

There are two LEDs on the Sno Processor Board. An RX LED and a STAT LED.

The RX LED is along the upper left side of the board, the STAT LED is on the upper right side of the board

  • RX LED - The RX LED indicates activity on the USB serial port.

  • STAT LED - A STAT LED is added to the top side of the board. This is useful debugging or as a status indicator.

MicroMod Alorium Sno M2 Processor Pin Functionality

The complete pin map is shown here or you can refer to the schematic. You can also download the PDF version of the pin map here.

Alorium's pin map

Click on image for a closer view of the pin map.
Pin Map courtesy of Alorium Technology

Board Dimensions

The board takes advantage of the standard MicroMod form factor.

Board Measures 1" x 1"