LP55231 Breakout Board Hookup Guide

≡ Pages
Contributors: Byron J.

Arduino Library

We've written an Arduino library to control the LP55231. It consists of two classes, which allow different degrees of control over the IC.

  • The Lp55231 class provides simple LED control.
  • the Lp55231Engines class extends the Lp55231 class, adding more sophisticated LP55231 features, such as the execution engines, and internal diagnostics, though also consuming more flash memory to do it.

We'll explore both classes in the following examples.