LilyPad USB Plus Hookup Guide

≡ Pages
Contributors: Gella

Uploading Code

Once you've installed the LilyPad USB Plus extensions to Arduino, you're ready to start programming the board!

Note that you won't have to install the extensions again, but you will need to perform the below three steps every time you want to program the board. These three steps are:

1. Connect the LilyPad USB Plus to your computer using a USB cable
2. Select "LilyPad USB Plus" from Arduino's "Board" menu
3. Select "LilyPad USB Plus" from Arduino's "Port" menu

Let's go over the three steps in detail:

1. Connect the LilyPad USB Plus to Your Computer

Place the LilyPad USB Plus on a clean, non-metal work surface. Connect the LilyPad USB Plus to a USB port on your computer using a micro-B USB cable. The cable can only be inserted one way, and should snap in securely.

USB Cable

Tip: Both the micro-B USB cable and the connector on the LilyPad have a subtle "D" shape to them. Match this shape to plug it in properly.

Connected to computer's USB port

Slide the switch on the LilyPad USB Plus to the ON position. You will not be able to upload code to the board if it is set to the OFF position.

Turn LilyPad USB Plus on

2. Select LilyPad USB Plus from the Board Menu

If the Arduino board support was installed correctly, "LilyPad USB Plus" option will be available in the Tools > Board list under the SparkFun AVR Boards group. Open the menu and select LilyPad USB Plus. Depending on how many boards are already in the list, you may need to scroll down a bit to get to it. A dot (Windows) or check mark (Mac) will show next to the board in the menu when it is selected, and it will show next to Board in the Tools menu.

IMPORTANT: You'll see some LilyPad entries higher in the Arduino menu, but the LilyPad USB Plus is not one of them. You'll need to scroll down to the SparkFun section at the bottom of the list to find it. We're working on getting the LilyPad USB Plus added to the LilyPad group in the future.

Select Board Definition

Troubleshooting: If you don't see "LilyPad USB Plus" in the board list, go back to Setting Up Arduino and double check that you performed all the steps. You might try restarting Arduino as well.

3. Select LilyPad USB Plus from the Port Menu

Arduino needs to know which port your LilyPad USB Plus is attached to so it can program it. Whenever you plug a USB device into your computer, your computer will assign it a port number. This used to be difficult to determine, but this board has a handy feature that identifies itself. Go to the Tools > Port menu, and select the port that has "LilyPad USB Plus" next to it.

On Windows, ports are listed as COM##; on a Mac or Linux machine they will be "/dev/cu.usbmodem####". Your screen may look different than the image below, depending on what operating system you are using, but all should show LilyPad USB Plus next to the port address.

COM Port

Troubleshooting: If you don't see a port with "LilyPad USB Plus" next to it, ensure that the board is powered up (switch in the ON position), and that the USB cable is securely connected to both the board and your computer. Some micro-USB cables are only meant for charging and don't pass data - they'll power the board, but it won't show up in the port menu. If needed, try a different cable.

Uploading Code

To review, once you've:

  1. Connected the LilyPad USB Plus to your computer using a USB cable.
  2. Selected the board type ("LilyPad USB Plus" NOT "LilyPad Arduino USB").
  3. Selected the COM port.

You are ready to upload code! Let's upload some code to try it out:

Load the "Blink" example from the menu File > Examples > 01.Basics > Blink. This is a very simple example program; it just blinks a LED on and off once per second.

Blink Example

Click the "Upload" button (the large round button with the right arrow in it).

Upload Button

Arduino will compile the code, then send it to the LilyPad USB Plus via the USB cable. While the code is uploading, the built-in LED will blink to signal the code is transferring. When the code finally runs, the RGB LED at the center of the board will slowly blink green. Success!

If this all works, congratulations! You're all set up and ready to prototype with the LilyPad USB Plus.

Troubleshooting: Error Messages on Upload?

If you are using a Mac and get an error message like the following:

Board LilyPad USB Plus (platform avr, package SparkFun) is unknown

It is possible that old Arduino versions left over after updates are interfering with the LilyPad USB Plus support installation. If you want to clear out this old information, follow these steps:

  1. Open Arduino's "Preferences" window.
  2. At the bottom of the window will be a link to your preferences file. Click on it and it will open a finder window.
  3. In the finder window, look for an "Arduino15" folder and delete it.
  4. Now open a finder window and open your personal folder (the one with your login name and a house icon next to it). Look for an "Arduino" folder (possibly in "Documents"). If the "Arduino" folder contains a "Hardware" folder, delete it. Your Arduino installation is now clean. Restart Arduino and repeat the LilyPad installation instructions from the previous page.

Troubleshooting: Still Problems Uploading?

If you still have problems uploading code to the LilyPad USB Plus and they are not outlined here, try checking out the troubleshooting section of our activity guide: