Getting Started with Walabot

≡ Pages
Contributors: bboyho

Hardware Assembly

Walabot Starter

To connect the Walabot Starter, you will need to align the "D" shape of the micro-B USB cable with the port.

Connect Walabot Starter to to your Computer with a micro-B Cable

Once the cable is connected to the Walabot, connect the other end to a computer's USB port.

Walabot Developer

To connect the Walabot Developer, insert the USB cable's micro-B end to the Walabot's USB port. You can use a separate micro-B USB 2.0 cable or the included micro-B USB 3.0 cable. By default, there is a jumper that uses the port closest to the edge of the Walabot.

Connecting with a separate micro-B USB 2.0 cable. Connecting with the included micro-B USB 3.0 cable.

If you decide to use a separate micro-B USB 2.0 cable to your computer, you will be aligning it with the "D" shape of the micro-B USB 3.0 connector as shown in the image below.

Close up of micro-B USB 2.0 Cable to micro-B USB 3.0 Cable

Once the cable is connected to the Walabot, connect the other end to a computer's USB port.

Mounting

You may want to mount the board during testing. Grab some electrical tape or mount the Walabot Starter to a box using standoffs. The Walabot Developer includes a magnetic disk that is able to stick to a surface such as a robot, smartphone, or wall. With the magnetic mount, it is able to attach and detach easily from the surface. In the examples provided, the starter and developer were mounted on a red box or resting on a table for testing.