Getting Started with the A111 Pulsed Radar Sensor

≡ Pages
Contributors: jimblom, bboyho, Elias The Sparkiest

Hardware Assembly

The A111 Pulsed Radar Breakout is designed to sit directly on top of a Raspberry Pi. Again, it doesn't span all 40 (2x20) pins of a Raspberry Pi B+ (or later), but the 26-pin — 2x13 — header should be compatible with any Pi.

Connect the shield to a Raspberry Pi ensuring that the "Pi Display" text on the breakout matches up with the display header on your Pi. The sensor should be facing up after plugging it in.

A111 HAT Stacked on a Raspberry Pi A111 HAT Stacked on a Raspberry Pi
A111 HAT v1.1 and v1.0 Stacked on a Raspberry Pi

Or, if you'd like to manually wire the breakout up to a Raspberry Pi's standard pinout, here is the pin-out we'll use through the rest of this tutorial. As stated in the hardware overview for v1.1, the input voltage is labeled as VIN while 1.0 labels the pin as 5V. Both pins are connected to 5V of the Raspberry Pi's HAT standard pinout. For v1.1, the additional PTH for VCCIO is included between the enable and GND pin.

v1.1 Breakout Pinv1.0 Breakout PinRaspberry Pi Pin NameRasPi Hardware Pin Number
CSCSSPI0 CS024
SCLKSCLKSPI0 SCLK23
MISOMISOSPI0 MISO21
MOSIMOSISPI0 MOSI19
INTINTGPIO2522
ENENGPIO2713
VCCIO3.3V1, 17
GNDGNDGND6, 14, 20, etc.
VIN5V5V2, 4