Galileo Experiment Guide
This Tutorial is Retired!
This tutorial covers concepts or technologies that are no longer current. It's still here for you to read and enjoy, but may not be as useful as our newest tutorials.
Introduction
Ready to learn the basics and see your Galileo in action? The Galileo board is software-compatible with the Arduino Software Development Environment, which makes getting started a snap. From building simple circuits to creating a Simon Says game, you will have a better understanding on how to build circuits and how to work with the Galileo. With these skills you can then create your own awesome project!
In this SparkFun Inventor's Kit for Galileo guide, you will learn the following:
Experiment List:
- SIK Galileo - Part 1: Blinking an LED
- SIK Galileo - Part 2: Reading a Potentiometer
- SIK Galileo - Part 3: Driving and RGB LED
- SIK Galileo - Part 4: Driving Multiple LEDs
- SIK Galileo - Part 5: Push Buttons
- SIK Galileo - Part 6: Reading a Photoresistor
- SIK Galileo - Part 7: Reading a Temperature Sensor
- SIK Galileo - Part 8: Driving a Servo Motor
- SIK Galileo - Part 9: Using a Flex Sensor
- SIK Galileo - Part 10: Reading a Soft Potentiometer
- SIK Galileo - Part 11: Using a Piezo Buzzer
- SIK Galileo - Part 12: Driving a Motor
- SIK Galileo - Part 13: Using Relays
- SIK Galileo - Part 14: Using a Shift Register
- SIK Galileo - Part 15: Using an LCD
- SIK Galileo - Part 16: Simon Says
Parts Needed
If you are following through all of the SIK Galileo tutorials we suggest getting these parts:
Required Reading
- Galileo Getting Started Guide - If your Galileo is fresh out of the box and you are just getting started, then we highly recommend you start here first.
Suggested Reading
Before continuing on with this tutorial, we recommend you be somewhat familiar with the concepts in the following tutorial:
- How to Use a Breadboard - First time working with a breadboard? Please check out this tutorial! It will help you understand why the breadboard is a great for prototyping and how to use one.