Galileo Experiment Guide

This Tutorial is Retired!

This tutorial covers concepts or technologies that are no longer current. It's still here for you to read and enjoy, but may not be as useful as our newest tutorials.

≡ Pages
Contributors: HelloTechie

SIK Galileo - Part 11: Using a Piezo Buzzer

Introduction

In this circuit, we'll again bridge the gap between the digital world and the analog world. We'll be using a piezo buzzer that makes a small "click" when you apply voltage to it (try it!). By itself that isn't terribly exciting, but if you turn the voltage on and off hundreds of times a second, the piezo buzzer will produce a tone. And if you string a bunch of tones together, you've got music! This circuit and sketch will play a classic tune. We'll never let you down!

Parts Needed

You will need the following parts:

  • 1x Breadboard
  • 1x Galileo
  • 1x Piezo Buzzer
  • 3x Jumper Wires

If you are following through all of the SIK Galileo tutorials we suggest using these parts:

Breadboard - Self-Adhesive (White)

PRT-12002
$6.25

Jumper Wires Standard 7" M/M - 30 AWG (30 Pack)

PRT-11026
$3.50

Mini Speaker - PC Mount 12mm 2.048kHz

COM-07950
$2.50

Intel® Galileo

DEV-12720
Retired

View the SparkFun Inventor's Kit for Galileo wishlist, to see the parts needed to go through the all the experiments.

Hardware Hookup

Ready to start hooking everything up? Check out the Fritzing diagram below, to see how everything is connected. Pay special attention to the component’s markings indicating how to place it on the breadboard. Polarized components can only be connected to a circuit in one direction.

Fritzing Diagram

Fritzing Diagram

Having a hard time seeing the circuit? Click on the Fritzing diagram to see a bigger image.

Code To Note

char notes[] = "cdfda ag cdfdg gf ";

char names[] = {'c','d','e','f','g','a','b','C'};

Up until now we've been working solely with numerical data, but the Arduino can also work with text. Characters (single, printable, letters, numbers and other symbols) have their own type, called "char". When you have an array of characters, it can be defined between double-quotes (also called a "string"), OR as a list of single-quoted characters.

tone(pin, frequency, duration);

One of Arduino's many useful built-in commands is the tone() function. This function drives an output pin at a certain frequency, making it perfect for driving buzzers and speakers. If you give it a duration (in milliseconds), it will play the tone then stop. If you don't give it a duration, it will keep playing the tone forever (but you can stop it with another function, noTone() ).

**Copy and paste the following code into the Arduino IDE. Hit upload and see what happens! **

/*
SparkFun Inventor's Kit Galileo
Example sketch 11

BUZZER

  Use the buzzer to play a song!

  The buzzer in your Inventor's Kit is an electromechanical
  component you can use to make noise. Inside the buzzer is a
  coil of wire and a small magnet. When current flows through 
  the coil, it becomes magnetized and pulls towards the magnet,
  creating a tiny "click". When you do this thousands of times
  per second, you create tones.

  The Arduino has a built-in command called tone() which clicks
  the buzzer at a certain frequency. This sketch knows the
  frequencies of the common notes, allowing you to create songs.
  We're never going to let you down!

Hardware connections:

  The buzzer has two pins. One is positive and one is negative.
  The postitive pin is marked by a "+" symbol on both the top
  and bottom of the buzzer.

  Connect the positive pin to Arduino digital pin 9.
  (Note that this must be a PWM pin.)
  Connect the negative pin to GND.

  Tip: if the buzzer doesn't fit into the breadboard easily,
  try rotating it slightly to fit into diagonal holes.

This sketch was written by SparkFun Electronics,
with lots of help from the Arduino community.
(This sketch was originally developed by D. Cuartielles for K3)
This code is completely free for any use.
Visit http://learn.sparkfun.com/products/2 for SIK information.
Visit http://www.arduino.cc to learn about the Arduino.

Version 2.0 6/2012 MDG
*/

/*
This sketch uses the buzzer to play songs.
The Arduino's tone() command will play notes of a given frequency.
We'll provide a function that takes in note characters (a-g),
and returns the corresponding frequency from this table:

  note  frequency
  c     262 Hz
  d     294 Hz
  e     330 Hz
  f     349 Hz
  g     392 Hz
  a     440 Hz
  b     494 Hz
  C     523 Hz

For more information, see http://arduino.cc/en/Tutorial/Tone
*/

const int buzzerPin = 9;

// We'll set up an array with the notes we want to play
// change these values to make different songs!

// Length must equal the total number of notes and spaces 

const int songLength = 18;

// Notes is an array of text characters corresponding to the notes
// in your song. A space represents a rest (no tone)

char notes[] = "cdfda ag cdfdg gf "; // a space represents a rest

// Beats is an array of values for each note and rest.
// A "1" represents a quarter-note, 2 a half-note, etc.
// Don't forget that the rests (spaces) need a length as well.

int beats[] = {1,1,1,1,1,1,4,4,2,1,1,1,1,1,1,4,4,2};

// The tempo is how fast to play the song.
// To make the song play faster, decrease this value.

int tempo = 150;


void setup() 
{
  pinMode(buzzerPin, OUTPUT);
}


void loop() 
{
  int i, duration;

  for (i = 0; i < songLength; i++) // step through the song arrays
  {
    duration = beats[i] * tempo;  // length of note/rest in ms

    if (notes[i] == ' ')          // is this a rest? 
    {
      delay(duration);            // then pause for a moment
    }
    else                          // otherwise, play the note
    {
      tone(buzzerPin, frequency(notes[i]), duration);
      delay(duration);            // wait for tone to finish
    }
    delay(tempo/10);              // brief pause between notes
  }

  // We only want to play the song once, so we'll pause forever:
  while(true){}
  // If you'd like your song to play over and over,
  // remove the above statement
}


int frequency(char note) 
{
  // This function takes a note character (a-g), and returns the
  // corresponding frequency in Hz for the tone() function.

  int i;
  const int numNotes = 8;  // number of notes we're storing

  // The following arrays hold the note characters and their
  // corresponding frequencies. The last "C" note is uppercase
  // to separate it from the first lowercase "c". If you want to
  // add more notes, you'll need to use unique characters.

  // For the "char" (character) type, we put single characters
  // in single quotes.

  char names[] = { 'c', 'd', 'e', 'f', 'g', 'a', 'b', 'C' };
  int frequencies[] = {262, 294, 330, 349, 392, 440, 494, 523};

  // Now we'll search through the letters in the array, and if
  // we find it, we'll return the frequency for that note.

  for (i = 0; i < numNotes; i++)  // Step through the notes
  {
    if (names[i] == note)         // Is this the one?
    {
      return(frequencies[i]);     // Yes! Return the frequency
    }
  }
  return(0);  // We looked through everything and didn't find it,
              // but we still need to return a value, so return 0.
}

What You Should See

You should see - well, nothing! But you should be able to hear a song. If it isn't working, make sure you have assembled the circuit correctly and verified and uploaded the code to your board or see the troubleshooting section.

Galileo Buzzer

Real World Application

Many modern megaphones have settings that use a loud amplified buzzer. They are usually very loud and quite good at getting people’s attention.

Troubleshooting

No Sound

Given the size and shape of the piezo buzzer it is easy to miss the right holes on the breadboard. Try double checking its placement.

Can't Think While the Melody is Playing

Just pull up the piezo buzzer whilst you think, upload your program then plug it back in.

Feeling Let Down and Deserted

The code is written so you can easily add your own songs.