Experiment Guide for RedBot with Shadow Chassis

≡ Pages
Contributors: bri_huang, Shawn Hymel, SFUptownMaker

Hardware

RedBot Mainboard

The RedBot Mainboard was designed to be as versatile as possible. It has banks of 3-pin I/O break-outs for easily connecting up LEDs, sensors, or motors. It also has an integrated H-Bridge Driver chip. We have developed an integrated library for the RedBot, if you want to drive the motors manually.

The RedBot mainboard, labeled for convenient reference

Here are the pin outs for the Motor Driver:

LEFT MOTOR:

  • Control 1 - Pin 2
  • Control 2 - Pin 4
  • Motor PWM (Speed) - Pin 5

RIGHT MOTOR:

  • Control 1 - Pin 7
  • Control 2 - Pin 8
  • Motor PWM (Speed) - Pin 6

Here's a quick tour of the hardware that's on the board:

  1. Analog/digital headers - These three headers provide one I/O pin, which can be used for analog input as well as digital input or output, as well as 5V power and ground. In addition, the header with A4 and A5 can be used for connecting I2C devices; the RedBot Accelerometer is designed to solder directly to this header, making connecting an accelerometer a snap.

  2. Analog input header - This header provides an additional two analog input pins. These pins can't be used for digital signals, however.

  3. Analog output/digital header - These two headers provide four pins which can be used for either PWM output or regular digital I/O. Note that the power supply for these headers is connected directly to the battery, providing extra umph for servo motors, but devices expecting 5V should not be connected directly to them!

  4. Wireless Socket - The RedBot has a socket for an XBee module, providing easy wireless interfacing.

  5. XBee Mode Switch A switch allows you to select whether the XBee communicates via the standard serial I/O pins (0 and 1, accessible through the built in Serial command set) or via pins 14 and 15 (A0 and A1), using the SoftwareSerial library. Using the software mode will consume two of your analog inputs, however.

  6. 5V / GND Headers - Headers are available to allow the user to tap off the 5V and ground signals.

  7. Power Switch - A power switch puts the board into a very low power consumption mode (microamps or less) allowing you to turn the board off without pulling the power connection.

  8. Motor Disable Switch - A motor disable switch allows you to turn off the motor driver so you can program the board without having it drive all over.

  9. Motor Headers - Headers are available to easily connect up the right and left side motors. The motor control is powered by the TB6612FNG Motor Driver.

  10. Power Input Header - A header has also been provided to allow you to access the input supply, either for purposes of driving additional circuitry or to allow more flexibility than the standard barrel jack does for power sources.

  11. DEBUG LED (pin 13) - An LED is connected to pin 13 to allow basic sanity checks that code is loading and running on the board.

  12. Power LED - A power LED will remain lit whenever the power switch is active.

Shadow Chassis

RedBot Chassis Complete Build

The Shadow Chassis is an economical robot platform with a lot of versatility. It features two gearmotors with 65mm wheels and a caster. The chassis pieces are made of ABS plastic with a wide variety of mounting holes for sensors, controllers, power, etc. Instructions for assembling the chassis can be found here.

RedBot Line Follower Sensor

Line sensor

The Line Follower sensor is an add-on for your RedBot that gives your robot the ability to detect lines or nearby objects. The sensor works by detecting reflected light coming from its own infrared LED. By measuring the amount of reflected infrared light, it can detect transitions from light to dark (lines) or even objects directly in front of it.

The sensor has a 3-pin header which connects directly to the RedBot Mainboard via female to female jumper wires. Use the included RedBot library to detect lines or objects. A mounting slot lets you easily connect one or more of these to the front or back of your robot chassis.

RedBot Accelerometer

Accelerometer

The Accelerometer sensor is an add-on for your RedBot that provides bump and motion detection. The sensor works by measuring acceleration forces on the x, y, and z axis. By measuring the amount of acceleration (or lack there of) your robot can get a better understanding of its movements.

The sensor has a 2x3 unpopulated footprint which connects directly to the RedBot Mainboard via a female header. You can also solder the sensor directly to the headers on the Mainboard if you wish.

RedBot Whisker Bumper

Bumper board

The Whisker Bumper is a very simple sensor comprised of a piece of music wire that closes a contact when bent and a circuit board to interface it to the RedBot. We ship the music wire straight, so you'll have to bend it to suit your application.

RedBot Buzzer Board

Buzzer

What's the fun of a robot that doesn't make beep-beep noises? We've made the RedBot Buzzer board to fit nicely on any header on the board, so you can integrate noise with your robot either just for fun or as a nice remote feedback function.

There's no special library support needed; just use the tone() family of commands already built into Arduino. One note: you can't use the Buzzer board on pins A6 and A7, as they are analog input-only pins.