ESP32-S2 Thing Plus Hookup Guide

≡ Pages
Contributors: QCPete, santaimpersonator

Introduction

The ESP32-S2 Thing Plus is a feather form-factor development board with the improved ESP32-S2 module, from Espressif. The new ESP32-S2 module addresses the security flaws in the original ESP32. While the ESP32-S2 does include improved security features, it lacks the Bluetooth capabilities of the original ESP32 module.

SparkFun Thing Plus - ESP32-S2 WROOM

WRL-17743
$24.50

Not Yet Implemented: The Arduino core for the ESP32 microcontroller are still a work in progress. There are a handful of peripherals and features that have yet to be implemented, including:

The peripherals are available (if, also, still in their infancy) in the IoT Development Framework for the ESP32. If your application requires any of the features above, consider giving the ESP-IDF a try! (Updated: June 2022.)

Required Materials

To get started, users will need a few items. Now some users may have a few of these items, feel free to modify your cart accordingly.

  • ESP32-S2 Thing Plus
  • USB 3.1 Cable A to C - 3 Foot - The USB interface serves two purposes: it powers the board and allows you to upload programs to it. (*If your computer doesn't provide a USB-A slot, then you will need to choose an appropriate cable or purchase an adapter as well.)
  • Computer with the an operating system (OS) that is compatible with all the software installation requirements.

SparkFun Thing Plus - ESP32-S2 WROOM

WRL-17743
$24.50

USB 3.1 Cable A to C - 3 Foot

CAB-14743
$7.95

Click the buttons above to toggle the additional materials based on the options you
wish to use. Feel free to modify the items in your cart to fit your needs.


Li-Po Battery

For mobile applications, users will want to pick up a single-cell LiPo battery from our catalog. Below, are a few available options:

Lithium Ion Battery - 400mAh

PRT-13851
$7.98

Lithium Ion Battery - 2Ah

PRT-13855
$19.41

Lithium Ion Battery - 110mAh

PRT-13853
$7.53

Lithium Ion Battery - 1Ah

PRT-13813
Retired

Jumper Modification

To modify the jumpers, users will need soldering equipment and/or a knife.

Solder Lead Free - 100-gram Spool

TOL-09325
$24.95

Chip Quik No-Clean Flux Pen - 10mL

TOL-14579
$8.50

Hobby Knife

TOL-09200
$3.75

Weller WLC100 Soldering Station

TOL-14228
Retired

Headers & Accessories

Headers are great for development purposes, letting users swap parts with just a set of jumper wires. If you would like to add headers to your board, check out some of the options for the Thing Plus or Feather form factor boards below. For a full selection of our available Headers or Soldering Tools, click on the associated links.

Straight Header - Male (PTH, 0.1in., 40-Pin)

PRT-00116
$1.95

Feather Stackable Header Set

PRT-15187
$2.25

Straight Header - Female (PTH, 0.1in., 8-Pin)

PRT-11895
$0.80

Straight Header - Female (PTH, 0.1in., 12-Pin)

PRT-14321
$0.80

SparkFun Beginner Tool Kit

TOL-14681
Retired

New to soldering? Check out our Through-Hole Soldering Tutorial for a quick introduction!

How to Work with Jumper Pads and PCB Traces

April 2, 2018
Handling PCB jumper pads and traces is an essential skill. Learn how to cut a PCB trace, add a solder jumper between pads to reroute connections, and repair a trace with the green wire method if a trace is damaged.

JTAG Functionality

Users interested in JTAG applications (i.e. programming and debugging the ESP32) will need an JTAG Programmer and need to solder on a JTAG header. We recommend these programmers from our catalog:

Straight Header - Male (PTH, 0.05in., 2x5-Pin)

PRT-15362
$1.95

J-Link EDU Mini Programmer

PGM-15345
Retired

J-Link EDU Base Programmer

PGM-15346
Retired

J-Link BASE Compact Programmer

PGM-15347
Retired
JTAG 20 Pin 0.1 In. To 10 Pin 0.05 In. Adapter

JTAG 20 Pin 0.1 In. To 10 Pin 0.05 In. Adapter

PGM-18421
Retired

Suggested Reading

As a more professionally oriented product, we will skip over the more fundamental tutorials (i.e. Ohm's Law and What is Electricity?). However, below are a few tutorials that may help users familiarize themselves with various aspects of the board.

How to Solder: Through-Hole Soldering

This tutorial covers everything you need to know about through-hole soldering.

Serial Communication

Asynchronous serial communication concepts: packets, signal levels, baud rates, UARTs and more!

Serial Peripheral Interface (SPI)

SPI is commonly used to connect microcontrollers to peripherals such as sensors, shift registers, and SD cards.

Pulse Width Modulation

An introduction to the concept of Pulse Width Modulation.

Logic Levels

Learn the difference between 3.3V and 5V devices and logic levels.

I2C

An introduction to I2C, one of the main embedded communications protocols in use today.

Analog vs. Digital

This tutorial covers the concept of analog and digital signals, as they relate to electronics.

How to Work with Jumper Pads and PCB Traces

Handling PCB jumper pads and traces is an essential skill. Learn how to cut a PCB trace, add a solder jumper between pads to reroute connections, and repair a trace with the green wire method if a trace is damaged.

Installing Arduino IDE

A step-by-step guide to installing and testing the Arduino software on Windows, Mac, and Linux.

ESP32 Thing Plus Hookup Guide

Hookup guide for the ESP32 Thing Plus (Micro-B) using the ESP32 WROOM's WiFi/Bluetooth system-on-chip in Arduino.

Installing Board Definitions in the Arduino IDE

How do I install a custom Arduino board/core? It's easy! This tutorial will go over how to install an Arduino board definition using the Arduino Board Manager. We will also go over manually installing third-party cores, such as the board definitions required for many of the SparkFun development boards.

Qwiic Connect System

One of the new, advanced features of the board is that it takes advantage of the Qwiic connect system. We recommend familiarizing yourself with the Logic Levels and I2C tutorials. Click on the banner above to learn more about Qwiic products.