ESP32 Environment Sensor Shield Hookup Guide

≡ Pages
Contributors: SFUptownMaker

Software

Besides the ESP32 Arduino Core, the ESP32 Environment Sensor Shield also requires the CCS811, BME280 and APDS-9301 Arduino libraries. Be sure to grab the libraries from each respective GitHub repositories, or you can download the files directly from the buttons below:

Note: This example assumes you are using the latest version of the Arduino IDE on your desktop. If this is your first time using Arduino, please review our tutorial on installing the Arduino IDE. If you have not previously installed an Arduino library, please check out our installation guide.

If you have not already, make sure to setup your own weather station with Wunderground. You will need to fill out a form and pick a username & password in order to receive a station ID. Sensor data from the ESP32 Thing and the ESP32 Environment Sensor Shield can then be pushed to Wunderground's server.

Here we present some example code for the ESP32 Environment Sensor Shield. This code reads all of the sensors, prints the resulting data to the serial port once per second, then posts some of the more germane data to Weather Underground once per minute.

language:c
#include <SparkFunCCS811.h>
#include "SparkFunBME280.h"
#include "Wire.h"
#include <Sparkfun_APDS9301_Library.h>
#include <WiFi.h>

BME280 bme;
CCS811 ccs(0x5B);
APDS9301 apds;

// Variables for wifi server setup 
const char* ssid     = "your_ssid_here";
const char* password = "password"; 
String ID = "wunderground_station_id";
String key = "wunderground_station_key";  
WiFiClient client;
const int httpPort = 80;
const char* host = "weatherstation.wunderground.com";

// Variables and constants used in calculating the windspeed.
volatile unsigned long timeSinceLastTick = 0;
volatile unsigned long lastTick = 0;

// Variables and constants used in tracking rainfall
#define S_IN_DAY   86400
#define S_IN_HR     3600
#define NO_RAIN_SAMPLES 2000
volatile long rainTickList[NO_RAIN_SAMPLES];
volatile int rainTickIndex = 0;
volatile int rainTicks = 0;
int rainLastDay = 0;
int rainLastHour = 0;
int rainLastHourStart = 0;
int rainLastDayStart = 0;
long secsClock = 0;

String windDir = "";
float windSpeed = 0.0;

// Pin assignment definitions
#define WIND_SPD_PIN 14
#define RAIN_PIN     25
#define WIND_DIR_PIN 35
#define AIR_RST      4
#define AIR_WAKE     15
#define DONE_LED     5

void setup() 
{
  delay(5);    // The CCS811 wants a brief delay after startup.
  Serial.begin(115200);
  Wire.begin();

  pinMode(DONE_LED, OUTPUT);
  digitalWrite(DONE_LED, LOW);

  // Wind speed sensor setup. The windspeed is calculated according to the number
  //  of ticks per second. Timestamps are captured in the interrupt, and then converted
  //  into mph. 
  pinMode(WIND_SPD_PIN, INPUT);     // Wind speed sensor
  attachInterrupt(digitalPinToInterrupt(WIND_SPD_PIN), windTick, RISING);

  // Rain sesnor setup. Rainfall is tracked by ticks per second, and timestamps of
  //  ticks are tracked so rainfall can be "aged" (i.e., rain per hour, per day, etc)
  pinMode(RAIN_PIN, INPUT);     // Rain sensor
  attachInterrupt(digitalPinToInterrupt(RAIN_PIN), rainTick, RISING);
  // Zero out the timestamp array.
  for (int i = 0; i < NO_RAIN_SAMPLES; i++) rainTickList[i] = 0;

  // BME280 sensor setup - these are fairly conservative settings, suitable for
  //  most applications. For more information regarding the settings available
  //  for the BME280, see the example sketches in the BME280 library.
  bme.settings.commInterface = I2C_MODE;
  bme.settings.I2CAddress = 0x77;
  bme.settings.runMode = 3;
  bme.settings.tStandby = 0;
  bme.settings.filter = 0;
  bme.settings.tempOverSample = 1;
  bme.settings.pressOverSample = 1;
  bme.settings.humidOverSample = 1;
  bme.begin();

  // CCS811 sensor setup.
  pinMode(AIR_WAKE, OUTPUT);
  digitalWrite(AIR_WAKE, LOW);
  pinMode(AIR_RST, OUTPUT);
  digitalWrite(AIR_RST, LOW);
  delay(10);
  digitalWrite(AIR_RST, HIGH);
  delay(100);
  ccs.begin();

  // APDS9301 sensor setup. Leave the default settings in place.
  apds.begin(0x39);


  // Connect to WiFi network
  Serial.print("Connecting to ");
  Serial.println(ssid);

  WiFi.begin(ssid, password);

  while (WiFi.status() != WL_CONNECTED) {
      delay(500);
      Serial.print(".");
  }
  Serial.println("");
  Serial.println("WiFi connected");
  Serial.println("IP address: ");
  Serial.println(WiFi.localIP());

  // Visible WiFi connected signal for when serial isn't connected
  digitalWrite(DONE_LED, HIGH);
}

void loop() 
{
  static unsigned long outLoopTimer = 0;
  static unsigned long wundergroundUpdateTimer = 0;
  static unsigned long clockTimer = 0;
  static unsigned long tempMSClock = 0;

  // Create a seconds clock based on the millis() count. We use this
  //  to track rainfall by the second. We've done this because the millis()
  //  count overflows eventually, in a way that makes tracking time stamps
  //  very difficult.
  tempMSClock += millis() - clockTimer;
  clockTimer = millis();
  while (tempMSClock >= 1000)
  {
    secsClock++;
    tempMSClock -= 1000;
  }

  // This is a once-per-second timer that calculates and prints off various
  //  values from the sensors attached to the system.
  if (millis() - outLoopTimer >= 2000)
  {
    outLoopTimer = millis();

    Serial.print("\nTimestamp: ");
    Serial.println(secsClock);

    // Windspeed calculation, in mph. timeSinceLastTick gets updated by an
    //  interrupt when ticks come in from the wind speed sensor.
    if (timeSinceLastTick != 0) windSpeed = 1000.0/timeSinceLastTick;
    Serial.print("Windspeed: ");
    Serial.print(windSpeed*1.492);
    Serial.println(" mph");

    // Update temperature. This also updates compensation values used to
    //  calculate other parameters.
    Serial.print("Temperature: ");
    Serial.print(bme.readTempF(), 2);
    Serial.println(" degrees F");

    // Display relative humidity.
    Serial.print("%RH: ");
    Serial.print(bme.readFloatHumidity(), 2);
    Serial.println(" %");

    // Display pressure.
    Serial.print("Pres: ");
    Serial.print(bme.readFloatPressure() * 0.0002953);
    Serial.println(" in");

    // Calculate the wind direction and display it as a string.
    Serial.print("Wind dir: ");
    windDirCalc(analogRead(WIND_DIR_PIN));
    Serial.print("  ");
    Serial.println(windDir);

    // Calculate and display rainfall totals.
    Serial.print("Rainfall last hour: ");
    Serial.println(float(rainLastHour)*0.011, 3);
    Serial.print("Rainfall last day: ");
    Serial.println(float(rainLastDay)*0.011, 3);
    Serial.print("Rainfall to date: ");
    Serial.println(float(rainTicks)*0.011, 3);

    // Trigger the CCS811's internal update procedure, then
    //  dump the values to the serial port.
    ccs.readAlgorithmResults();

    Serial.print("CO2: ");
    Serial.println(ccs.getCO2());

    Serial.print("tVOC: ");
    Serial.println(ccs.getTVOC());

    Serial.print("Luminous flux: ");
    Serial.println(apds.readLuxLevel(),6);

    // Calculate the amount of rain in the last day and hour.
    rainLastHour = 0;
    rainLastDay = 0;
    // If there are any captured rain sensor ticks...
    if (rainTicks > 0)
    {
      // Start at the end of the list. rainTickIndex will always be one greater
      //  than the number of captured samples.
      int i = rainTickIndex-1;

      // Iterate over the list and count up the number of samples that have been
      //  captured with time stamps in the last hour.
      while ((rainTickList[i] >= secsClock - S_IN_HR) && rainTickList[i] != 0)
      {
        i--;
        if (i < 0) i = NO_RAIN_SAMPLES-1;
        rainLastHour++;
      }

      // Repeat the process, this time over days.
      i = rainTickIndex-1;
      while ((rainTickList[i] >= secsClock - S_IN_DAY) && rainTickList[i] != 0)
      {
        i--;
        if (i < 0) i = NO_RAIN_SAMPLES-1;
        rainLastDay++;
      }
      rainLastDayStart = i;
    }
  }

  // Update wunderground once every sixty seconds.
  if (millis() - wundergroundUpdateTimer >= 60000)
  {

  wundergroundUpdateTimer = millis();
    // Set up the generic use-every-time part of the URL
    String url = "/weatherstation/updateweatherstation.php";
    url += "?ID=";
    url += ID;
    url += "&PASSWORD=";
    url += key;
    url += "&dateutc=now&action=updateraw";

    // Now let's add in the data that we've collected from our sensors
    // Start with rain in last hour/day
    url += "&rainin=";
    url += rainLastHour;
    url += "&dailyrainin=";
    url += rainLastDay;

    // Next let's do wind
    url += "&winddir=";
    url += windDir;
    url += "&windspeedmph=";
    url += windSpeed;

    // Now for temperature, pressure and humidity.
    url += "&tempf=";
    url += bme.readTempF();
    url += "&humidity=";
    url += bme.readFloatHumidity();
    url += "&baromin=";
    float baromin = 0.0002953 * bme.readFloatPressure();
    url += baromin;

    // Connnect to Weather Underground. If the connection fails, return from
    //  loop and start over again.
    if (!client.connect(host, httpPort))
    {
      Serial.println("Connection failed");
      return;
    }
    else
    {
      Serial.println("Connection succeeded");
    }

    // Issue the GET command to Weather Underground to post the data we've 
    //  collected.
    client.print(String("GET ") + url + " HTTP/1.1\r\n" +
                 "Host: " + host + "\r\n" +
                 "Connection: close\r\n\r\n");

    // Give Weather Underground five seconds to reply.
    unsigned long timeout = millis();
    while (client.available() == 0) 
    {
      if (millis() - timeout > 5000) 
      {
          Serial.println(">>> Client Timeout !");
          client.stop();
          return;
      }
    }

    // Read the response from Weather Underground and print it to the console.
    while(client.available()) 
    {
      String line = client.readStringUntil('\r');
      Serial.print(line);
    }
  }
}

// Keep track of when the last tick came in on the wind sensor.
void windTick(void)
{
  timeSinceLastTick = millis() - lastTick;
  lastTick = millis();
}

// Capture timestamp of when the rain sensor got tripped.
void rainTick(void)
{
  rainTickList[rainTickIndex++] = secsClock;
  if (rainTickIndex == NO_RAIN_SAMPLES) rainTickIndex = 0;
  rainTicks++;
}

// For the purposes of this calculation, 0deg is when the wind vane
//  is pointed at the anemometer. The angle increases in a clockwise
//  manner from there.
void windDirCalc(int vin)
{
  if      (vin < 150) windDir="202.5";
  else if (vin < 300) windDir = "180";
  else if (vin < 400) windDir = "247.5";
  else if (vin < 600) windDir = "225";
  else if (vin < 900) windDir = "292.5";
  else if (vin < 1100) windDir = "270";
  else if (vin < 1500) windDir = "112.5";
  else if (vin < 1700) windDir = "135";
  else if (vin < 2250) windDir = "337.5";
  else if (vin < 2350) windDir = "315";
  else if (vin < 2700) windDir = "67.5";
  else if (vin < 3000) windDir = "90";
  else if (vin < 3200) windDir = "22.5";
  else if (vin < 3400) windDir = "45";
  else if (vin < 4000) windDir = "0";
  else windDir = "0";
}

Note: When connecting to a WiFi network and the Wunderground server, make sure to modify the variables ssid, password, ID, and key.

Expected Output

Here is a picture of what you should expect upon starting up your ESP32 and letting it connect to WiFi:

Initial startup picture

The first few lines are just diagnostics from the ESP32, and will be present at boot time regardless of the application being run. Immediately below the line "Connecting to sparkfun-guest" you see a series of dots. One dot appears every half second while the connection is pending, so you can see from this example that it took approximately 3 seconds for the WiFi to come online. After that, the various environmental parameters we're looking at are printed out, along with a timestamp in seconds since the platform was booted.

Once a minute, the stream of data from the sensors is interrupted by a connection to the weatherunderground.com servers. Here's what that output looks like:

Connecting to wunderground servers

There are two useful pieces of data here. The first, where it says "Connection succeeded", shows that a successful connection has been made to the Weather Underground server. If your internet connection is down, this will fail.

The second is the one lone line that says "success". This is the response from the server after your attempt to post data to it. If this fails, it means that you connected to the server, but the string you formatted to send to the server isn't formatted properly. This shouldn't be a problem unless you change the example code.