MicroMod SAMD51 Processor Board Hookup Guide

Pages
Contributors: bboyho, Elias The Sparkiest

Introduction

With the MicroMod specification, we shrunk down the PCB size for the SAMD51 32-bit ARM Cortex-M4F MCU! This tutorial covers the basic functionality of the MicroMod SAMD51 and highlights its features.

SparkFun MicroMod SAMD51 Processor

DEV-16791
$18.95

Required Materials

To follow along with this tutorial, you will need the following materials. You may not need everything though depending on what you have. Add it to your cart, read through the guide, and adjust the cart as necessary.

SparkFun MicroMod ATP Carrier Board

DEV-16885
$20.50

SparkFun Mini Screwdriver

TOL-09146
$1.50

USB 3.1 Cable A to C - 3 Foot

CAB-14743
$7.95

SparkFun MicroMod SAMD51 Processor

DEV-16791
$18.95

Suggested Reading

If you aren't familiar with the MicroMod ecosystem, we recommend reading here for an overview.

MicroMod Logo
MicroMod Ecosystem

If you aren’t familiar with the following concepts, we also recommend checking out these tutorials before continuing.

Serial Communication

Asynchronous serial communication concepts: packets, signal levels, baud rates, UARTs and more!

Serial Peripheral Interface (SPI)

SPI is commonly used to connect microcontrollers to peripherals such as sensors, shift registers, and SD cards.

Installing Arduino IDE

A step-by-step guide to installing and testing the Arduino software on Windows, Mac, and Linux.

Logic Levels

Learn the difference between 3.3V and 5V devices and logic levels.

I2C

An introduction to I2C, one of the main embedded communications protocols in use today.

Getting Started with MicroMod

Dive into the world of MicroMod - a compact interface to connect a microcontroller to various peripherals via the M.2 Connector!