SparkFun 9DoF IMU (ICM-20948) Breakout Hookup Guide

≡ Pages
Contributors: Ell C, Liquid Soulder

Introduction

The SparkFun 9DoF IMU Breakout incorporates all the amazing features of Invensense's ICM-20948 into a Qwiic-enabled breakout board replete with logic shifting and broken out GPIO pins for all your motion sensing needs. The ICM-20948 itself is an extremely low powered, I2C and SPI enabled 9-axis motion tracking device that is ideally suited for smartphones, tablets, wearable sensors, and IoT applications. Featuring a 3-Axis Gyroscope with four selectable ranges, a 3-Axis Accelerometer, again with four selectable ranges, a 3-axis compass with a wide range to ±4900 µT, and an on-board Digital Motion Processor, this little breakout can even detect the motion of invisibility cloaks. Not really. Just checking to see if you were still with me. But it is pretty amazing. Check it out:

SparkFun 9DoF IMU Breakout - ICM-20948 (Qwiic)

SEN-15335
Retired

In this hookup guide, we'll connect our sensor up to our Esp32 Thing Plus microcontroller and run a of quick (Qwiic) example to get you up and running with this fantastic board!

Required Materials

To follow along with this tutorial, you will need the following materials. You may not need everything though depending on what you have. Add it to your cart, read through the guide, and adjust the cart as necessary.

Tools

If you choose to utilize the broken out GPIO, you will need a soldering iron, solder, and general soldering accessories.

Soldering Iron - 60W (Adjustable Temperature)

TOL-14456
$25.95

Solder Lead Free - 15-gram Tube

TOL-09163
$4.95

Suggested Reading

If you aren't familiar with the Qwiic system, we recommend reading here for an overview.

Qwiic Connect System
Qwiic Connect System

We would also recommend taking a look at the following tutorials if you aren't familiar with them.

How to Solder: Through-Hole Soldering

This tutorial covers everything you need to know about through-hole soldering.

Accelerometer Basics

A quick introduction to accelerometers, how they work, and why they're used.

I2C

An introduction to I2C, one of the main embedded communications protocols in use today.

Serial Terminal Basics

This tutorial will show you how to communicate with your serial devices using a variety of terminal emulator applications.