RedBot Assembly Guide

This Tutorial is Retired!

This tutorial covers concepts or technologies that are no longer current. It's still here for you to read and enjoy, but may not be as useful as our newest tutorials.

≡ Pages
Contributors: SFUptownMaker, HelloTechie

RedBot MainBoard Standoffs

Since the battery holder is screwed down, it is now easier to add the metal L10 standoffs in the locations where the RedBot Mainboard will go.

Locate the following:

  • 4x M3*6 Screw
  • 4x L10 Metal Standoffs

Locate the following locations on the top chassis piece where you will add four L10 metal standoffs.

Stand offs for RedBot Mainboard

Using the M3*6 screws, add all four L10 metal standoffs on the top chassis piece with the L10 metal standoffs located on the same side as the battery holder.

All 4 stands on the top chassis piece