RedBot Assembly Guide

This Tutorial is Retired!

This tutorial covers concepts or technologies that are no longer current. It's still here for you to read and enjoy, but may not be as useful as our newest tutorials.

≡ Pages
Contributors: SFUptownMaker, HelloTechie

RedBot Line Followers

In this section, you will be putting standoffs on the RedBot Sensor - Line Followers. Then you will add the sensors on your chassis.

Locate the following:

  • 3x Line Followers
  • 3x 4-40 1" Phillips Screw
  • 3x 4-40 1/4" Phillips Screw
  • 6x 4-40 Nylon Standoffs

Screw a 4-40 1" Phillips screw to the plastic standoff through one of the RedBot Sensor - Line Followers. Make sure to tighten the standoff on the line follower's header side. The top of the screw should be on the same side as the RedBot Sensor - Line Follower's sensor. Do this for the other two RedBot Sensor - Line Followers.

Screw the plastic stand off

You should see part of the 4-40 1" Phillips screw sticking out.

alt text

You will screw on another standoff on top of the one already on the screw. The screw's end should now be covered as pictured below.

Place the second stand off on top

Do this for all other two RedBot Sensor - Line Followers.

Do for all three line followers

Locate three spots on the chassis where you will be adding the RedBot Sensor - Line Followers.

Line Follower location

Place a 4-40 1/4" Phillips screw through the top side of the chassis piece. Tighten down the standoff with a RedBot Sensor - Line Follower into bottom chassis piece. The RedBot Sensor - Line Follower should be on the bottom side of the chassis piece. The headers on the RedBot Sensor - Line Follower should be pointing in towards the chassis.

Screw into bottom chassis

Using your other two 4-40 1/4" Phillips screws, hand tighten the other two RedBot Sensor - Line Followers in the suggested locations.

Do for all three line followers