Qwiic Pro Micro USB-C (ATmega32U4) Hookup Guide

≡ Pages
Contributors: bboyho

Example 3: Qwiic Enabled HID Mouse and Keyboard

Note: If you have not previously installed an Arduino library, please check out our installation guide.

As another option, you can try to use a Qwiic device to take advantage of the HID class. We broke up the Qwiic HID examples into three parts. Depending on your application and personal preference, you could essentially use a different Qwiic enabled device.

Example 3a: HID Mouse with Qwiic Joystick

For the scope of this tutorial example, we will be using the Qwiic Joystick so that we do not need to solder any pins. Make sure to check out the Qwiic Joystick Hookup Guide before continuing on with the examples below.

Qwiic Joystick Hookup Guide

February 21, 2019
Looking for an easy way to implement a joystick to your next Arduino or Raspberry Pi project? This hookup guide will walk you through using the Qwiic Joystick with the Arduino IDE on a RedBoard Qwiic and in Python on a Raspberry Pi.

Copy and paste the code below into the Arduino IDE. Make sure to select the correct board and COM port that your respective board enumerated to.

language:c
/******************************************************************************
  Example_3a_Qwiic_Joystick_HID_Mouse.ino
  Written by: Ho Yun "Bobby" Chan
  Date: January 13, 2020
  Development Environment Specifics:
    Arduino IDE 1.8.9

  Description:
    Based on the Jim's Pro Micro "HID Mouse" and Wes' Qwiic Joystick "basic reading"
    examples, this example moves your computer's mouse based on the joystick's
    position. Pressing down on the joystick's will enable a mouse's left click.
    The left click will relese as soon as you stop pressing down on the joystick.

  Libraries:
    Mouse.h (included with Arduino IDE)
    Wire.h (included with Arduino IDE)
    SparkFun_Qwiic_Joystick_Arduino_Library.h (included in the src folder) http://librarymanager/All#SparkFun_joystick

  License:
    This code is released under the MIT License (http://opensource.org/licenses/MIT)

  ******************************************************************************/

#include <Mouse.h>
#include <Wire.h>

#include "SparkFun_Qwiic_Joystick_Arduino_Library.h" //Click here to get the library: http://librarymanager/All#SparkFun_joystick
JOYSTICK joystick;                                   //Create instance of this object

int vertZero, horzZero;       // Stores the initial value of each axis, usually around 512
int vertValue, horzValue;     // Stores current analog output of each axis
const int sensitivity = 200;  // Higher sensitivity value = slower mouse, should be <= about 500
int mouseClickFlag = 0;

//int invertMouse = 1;        //Invert joystick based on orientation
int invertMouse = -1;         //Noninverted joystick based on orientation

//Debug mode, comment one of these lines out using a syntax
//for a single line comment ("//"):
#define DEBUG 0       //0 = HID only
//#define DEBUG 1     //1 = HID with serial output

void setup() {
#if DEBUG
  Serial.begin(9600);
  Serial.println("Example 3: HID Mouse w/ Qwiic Joystick");
#endif

  if (joystick.begin() == false)
  {
#if DEBUG
    Serial.println("Joystick does not appear to be connected. Please check wiring. Freezing...");
#endif
    while (1);
  }

  delay(1000);  // short delay to let outputs settle
  vertZero = joystick.getVertical();  // get the initial values
  horzZero = joystick.getHorizontal();  // Joystick should be in neutral position when reading these

  Mouse.begin(); //Init mouse emulation
}

void loop() {
#if DEBUG
  Serial.print("X: ");
  Serial.print(joystick.getHorizontal());

  Serial.print(" Y: ");
  Serial.print(joystick.getVertical());

  Serial.print(" Button: ");
  Serial.println(joystick.getButton());
#endif

  vertValue = joystick.getVertical() - vertZero; // read vertical offset
  horzValue = joystick.getHorizontal() - horzZero;  // read horizontal offset

  if (vertValue != 0)
    Mouse.move(0, (invertMouse * (vertValue / sensitivity)), 0); // move mouse on y axis
  if (horzValue != 0)
    Mouse.move((invertMouse * (horzValue / sensitivity)), 0, 0); // move mouse on x axis

  if ((joystick.getButton() == 0) && (!mouseClickFlag))  // if the joystick button is pressed
  {
    mouseClickFlag = 1;
    Mouse.press(MOUSE_LEFT);  // click the left button down
  }
  else if ((joystick.getButton()) && (mouseClickFlag)) // if the joystick button is not pressed
  {
    mouseClickFlag = 0;
    Mouse.release(MOUSE_LEFT);  // release the left button
  }

  //delay(200); //remove "//" on this line if you need a small delay
}

Moving the Qwiic joystick will move your mouse on the screen. Pressing down on the button will cause a left mouse click. Once you stop pressing down on the joystick, it will release the left mouse click. Depending on the orientation for the vertical, you can invert the mouse's movement using the invertMouse variable at the beginning of the example code.

Example 3b: HID Keyboard with Qwiic Keypad

For the scope of this tutorial example, we will be using the Qwiic Keypad so that we do not need to solder any pins. Make sure to check out the Qwiic Keypad Hookup Guide before continuing on with the examples below.

Qwiic Keypad Hookup Guide

April 25, 2019
If you are tired of taking up GPIO pins, wiring a bunch of pull up resistors, and using firmware that scans the keys taking up valuable processing time... check out the new Qwiic Keypad.

Copy and paste the code below into the Arduino IDE. Make sure to select the correct board and COM port that your respective board enumerated to.

language:c
/******************************************************************************
  Example_3b_Qwiic_Keypad_HID_Keyboard.ino
  Written by: Ho Yun "Bobby" Chan
  Date: February 6, 2020
  Development Environment Specifics:
    Arduino IDE 1.8.9

  Description:
    Based on the Jim's Pro Micro "HID Mouse" and Pete' Qwiic Keypad "read button"
    examples, this example outputs keyboard presses associated with the keypad.

  Libraries:
   Keyboard.h (included with Arduino IDE)
   Wire.h (included with Arduino IDE)
   SparkFun_Qwiic_Keypad_Arduino_Library.h (included in the src folder) http://librarymanager/All#SparkFun_keypad

  License:
    This code is released under the MIT License (http://opensource.org/licenses/MIT)

******************************************************************************/

#include <Keyboard.h>
#include <Wire.h>
#include "SparkFun_Qwiic_Keypad_Arduino_Library.h" //Click here to get the library: http://librarymanager/All#SparkFun_keypad
KEYPAD keypad1;                                    //Create instance of this object

void setup() {
  Serial.begin(9600);
  Serial.println("Qwiic KeyPad Example");

  if (keypad1.begin() == false)   // Note, using begin() like this will use default I2C address, 0x4B.
    // You can pass begin() a different address like so: keypad1.begin(Wire, 0x4A).
  {
    Serial.println("Keypad does not appear to be connected. Please check wiring. Freezing...");
    while (1);
  }
  Serial.print("Initialized. Firmware Version: ");
  Serial.println(keypad1.getVersion());
  Serial.println("Press a button: * to do a space. # to go to next line.");

  Keyboard.begin(); //Init keyboard emulation
}

void loop() {
  keypad1.updateFIFO();  // necessary for keypad to pull button from stack to readable register
  char button = keypad1.getButton();

  if (button == -1)
  {
    Serial.println("No keypad detected");
    delay(1000);
  }
  else if (button != 0)
  {
    if (button == '0') {//note that this is a keypad '0' not the button press itself
      Keyboard.write('0');
    }
    else if (button == '1') {
      Keyboard.write('1');
    }
    else if (button == '2') {
      Keyboard.write('2');
    }
    else if (button == '3') {
      Keyboard.write('3');
    }
    else if (button == '4') {
      Keyboard.write('4');
    }
    else if (button == '5') {
      Keyboard.write('5');
    }
    else if (button == '6') {
      Keyboard.write('6');
    }
    else if (button == '7') {
      Keyboard.write('7');
    }
    else if (button == '8') {
      Keyboard.write('8');
    }
    else if (button == '9') {
      Keyboard.write('9');
    }
    else if (button == '#') {
      Keyboard.write('#');
    }
    else if (button == '*') {
      Keyboard.write('*');
    }
  }

  //Do something else. Don't call your Keypad a ton otherwise you'll tie up the I2C bus
  delay(25); //25 is good, more is better
}

If you have a text editor (Notepad, Word, TextEdit, etc.) open and active from Example 2, press a button on the Qwiic Keypad. Or you can try using the textbox below to test. The outputs should be associated with each of the Qwiic keypad button press.

Example 3c: Qwiic HID Mouse and Keyboard Combined

This example combines 3a and 3b into one sketch. Copy and paste the code below into the Arduino IDE. Make sure to select the correct board and COM port that your respective board enumerated to.

language:c
/******************************************************************************
  Example_3c_Qwiic_HID_Mouse_Keyboard_Combined.ino
  Written by: Ho Yun "Bobby" Chan
  Date: February 6, 2020
  Development Environment Specifics:
    Arduino IDE 1.8.9

  Description:
    Based on the following examples:
      - Jim's Pro Micro "HID Mouse/Keyboard"
      - Wes' Qwiic Joystick "basic reading"
      - Pete's Qwiic Keypad "read button"

    This example controls the mouse with the Qwiic Joystick
    and keyboard presses associated with the Qwiic Keypad.
    The serial output is turned off so that Qwiic Pro Micro
    can respond faster.

  Libraries:
   Mouse.h (included with Arduino IDE)
   Keyboard.h (included with Arduino IDE)
   Wire.h (included with Arduino IDE)
   SparkFun_Qwiic_Joystick_Arduino_Library.h (included in the src folder) http://librarymanager/All#SparkFun_joystick
   SparkFun_Qwiic_Keypad_Arduino_Library.h (included in the src folder) http://librarymanager/All#SparkFun_keypad

  License:
    This code is released under the MIT License (http://opensource.org/licenses/MIT)

******************************************************************************/

#include <Mouse.h>
#include <Keyboard.h>
#include <Wire.h>

#include "SparkFun_Qwiic_Joystick_Arduino_Library.h" //Click here to get the library: http://librarymanager/All#SparkFun_joystick
JOYSTICK joystick;                                   //Create instance of this object

#include "SparkFun_Qwiic_Keypad_Arduino_Library.h" //Click here to get the library: http://librarymanager/All#SparkFun_keypad
KEYPAD keypad1;                                    //Create instance of this object

int vertZero, horzZero;       // Stores the initial value of each axis, usually around 512
int vertValue, horzValue;     // Stores current analog output of each axis
const int sensitivity = 150;  // Higher sensitivity value = slower mouse, should be <= about 500
int mouseClickFlag = 0;

//int invertMouse = 1;        //Invert joystick based on orientation
int invertMouse = -1;         //Noninverted joystick based on orientation

//Debug mode, comment one of these lines out using a syntax
//for a single line comment ("//"):
#define DEBUG 0       //0 = HID only
//#define DEBUG 1     //1 = HID with serial output

void setup() {
#if DEBUG
  Serial.begin(9600);
  Serial.println("Qwiic KeyPad Example");
#endif

  if (joystick.begin() == false) {
#if DEBUG
    Serial.println("Joystick does not appear to be connected. Please check wiring. Freezing...");
#endif
    while (1);
  }
  if (keypad1.begin() == false) {  // Note, using begin() like this will use default I2C address, 0x4B.
    // You can pass begin() a different address like so: keypad1.begin(Wire, 0x4A).
#if DEBUG
    Serial.println("Keypad does not appear to be connected. Please check wiring. Freezing...");
#endif
    while (1);
  }

  delay(1000);  // short delay to let outputs settle
  vertZero = joystick.getVertical();  // get the initial values
  horzZero = joystick.getHorizontal();  // Joystick should be in neutral position when reading these

#if DEBUG
  Serial.print("Initialized. Firmware Version: ");
  Serial.println(keypad1.getVersion());
  Serial.println("Press a button: * to do a space. # to go to next line.");
#endif

  Mouse.begin(); //Init mouse emulation
  Keyboard.begin(); //Init keyboard emulation

}//end setup

void loop() {
  keypad1.updateFIFO();  // necessary for keypad to pull button from stack to readable register
  char button = keypad1.getButton();

#if DEBUG
  Serial.print("X: ");
  Serial.print(joystick.getHorizontal());

  Serial.print(" Y: ");
  Serial.print(joystick.getVertical());

  Serial.print(" Button: ");
  Serial.println(joystick.getButton());
#endif

  vertValue = joystick.getVertical() - vertZero; // read vertical offset
  horzValue = joystick.getHorizontal() - horzZero;  // read horizontal offset

  if (vertValue != 0)
    Mouse.move(0, (invertMouse * (vertValue / sensitivity)), 0); // move mouse on y axis
  if (horzValue != 0)
    Mouse.move((invertMouse * (horzValue / sensitivity)), 0, 0); // move mouse on x axis

  if ((joystick.getButton() == 0) && (!mouseClickFlag))  // if the joystick button is pressed
  {
    mouseClickFlag = 1;
    Mouse.press(MOUSE_LEFT);  // click the left button down
  }
  else if ((joystick.getButton()) && (mouseClickFlag)) // if the joystick button is not pressed
  {
    mouseClickFlag = 0;
    Mouse.release(MOUSE_LEFT);  // release the left button
  }

  if (button == -1) {
#if DEBUG
    Serial.println("No keypad detected");
#endif
    delay(1000);
  }

  else if (button != 0) {
#if DEBUG
    Serial.print("Qwiic Keypad Button:  ");
    Serial.println(button);
#endif
    if (button == '0') {//note that this is a keypad '0' not the button press itself
      Keyboard.write('0');
    }
    else if (button == '1') {
      Keyboard.write('1');
    }
    else if (button == '2') {
      Keyboard.write('2');
    }
    else if (button == '3') {
      Keyboard.write('3');
    }
    else if (button == '4') {
      Keyboard.write('4');
    }
    else if (button == '5') {
      Keyboard.write('5');
    }
    else if (button == '6') {
      Keyboard.write('6');
    }
    else if (button == '7') {
      Keyboard.write('7');
    }
    else if (button == '8') {
      Keyboard.write('8');
    }
    else if (button == '9') {
      Keyboard.write('9');
    }
    else if (button == '#') {
      Keyboard.write('#');
    }
    else if (button == '*') {
      Keyboard.write('*');
    }
  }

  //Do something else. Don't call your Keypad a ton otherwise you'll tie up the I2C bus
  //Uncomment this if necessary but since we check the Qwiic Joystick it does not
  // appear to be an issue
  //delay(25); //25 is good, more is better

}//end loop

The functionality should be the same when moving the joystick or pressing on the keypad's key. The serial output is turned off so that Qwiic Pro Micro can respond faster.