Qwiic LED Stick - APA102C Hookup Guide

≡ Pages
Contributors: El Duderino, MAKIN-STUFF

Resources and Going Further

That wraps up this tutorial for the Qwiic LED Stick. For more information on the board, take a look at the following resources:

For some inspiration on an LED project with the Qwiic LED Stick, take a look at these tutorials:

Das Blinken Top Hat

A top hat decked out with LED strips makes for a heck of a wedding gift.

Interactive LED Music Visualizer

Use an Arduino and the SparkFun Sound Detector to create visualizations on Addressable RGB LED strips.

LED Cloud-Connected Cloud

Make an RGB colored cloud light! You can also control it from your phone, or hook up to the weather!

LED Crystal Goddess Crown

Follow this tutorial to make your own Crystal Goddess Crown with LEDs!

LuMini Ring Hookup Guide

The LuMini Rings (APA102-2020) are the highest resolution LED rings available.

LuMini 8x8 Matrix Hookup Guide

The LuMini 8x8 Matrix (APA102-2020) are the highest resolution LED matrix available.

LumiDrive Hookup Guide

The LumiDrive LED Driver is SparkFun’s foray into all things Python on micro-controllers. With the SparkFun LumiDrive you will be able to control and personalize a whole strand of APA102s directly from the board itself.

Or check out some of these blog posts for ideas: