MicroMod GNSS Function Board - ZED-F9P Hookup Guide

≡ Pages
Contributors: El Duderino

Introduction

As some readers may guess by the assortment of SparkFun products featuring it, we love the ZED-F9P GNSS module from u-blox. The SparkFun MicroMod GNSS Function Board - ZED-F9P provides high precision GNSS capabilities for MicroMod projects using Main Board/Function Board assemblies. The ZED-F9P module from u-blox is capable of up to 10mm 3-dimensional accuracy though the module requires a clear view of the sky as well as correction data from an RTCM source to achieve this accuracy. The ZED-F9P can act as a base station as well so you can use it with a second Function Board (or another SparkFun ZED-F9P product) together to achieve millimeter positional accuracy.

SparkFun MicroMod GNSS Function Board - ZED-F9P

GPS-19663
$274.95 $184.22

Having the ZED-F9P on a MicroMod Function board allows for even more versatility with projects using the ZED-F9P allowing users to mix and match not only their preferred Processor but also to pair it with another Function Board to add even more versatility to a GNSS project.

This guide will go over the hardware present on this Function Board, how to assemble it into a MicroMod circuit as well as an Arduino example to start getting location data from the ZED-F9P.

Required Materials

You'll need the following materials along with the MicroMod GNSS Function Board - ZED-F9P to complete this tutorial and use the Function Board.

Main Board

All Function Boards require a Main Board and Processor to connect to each other. Depending on your application, you may need either a Single or Dual Main Board:

SparkFun MicroMod Main Board - Single

DEV-18575
Retired

SparkFun MicroMod Main Board - Double

DEV-18576
Retired

Processor Board

You'll need a Processor Board to act as a host controller for the Function Board:

SparkFun MicroMod Teensy Processor

DEV-16402
$24.95

SparkFun MicroMod ESP32 Processor

WRL-16781
$19.95

SparkFun MicroMod SAMD51 Processor

DEV-16791
Retired

SparkFun MicroMod Artemis Processor

DEV-16401
$17.50

Antenna

The GNSS Function Board also requires an antenna. We recommend using a GNSS multi-band antenna compatible with both L1 and L2 bands for full reception like the ones below:

GNSS L1/L2 Multi-Band Magnetic Mount Antenna - 5m (SMA)

GPS-15192
$109.95

GNSS Multi-Band L1/L2 Helical Antenna (SMA) BT-560

GPS-17383
Retired

Antenna Accessories

The GNNS Function Board uses a u.Fl connector for the antenna connection so in order to use the antennas listed above, you will need an adapter cable like the ones below. You may also want a grounding plate to maximize your antenna's reception:

RP-SMA to U.FL Cable - 150mm

WRL-18569
$2.75

Interface Cable SMA to U.FL - 100mm

WRL-09145
$5.75

GPS Antenna Ground Plate

GPS-17519
$7.25

Interface Cable U.FL to SMA - 100mm

WRL-18154
Retired

Suggested Reading

The MicroMod ecosystem is a unique way to allow users to customize their project to their needs. If you aren't familiar with the MicroMod system, click on the banner below for more information.

MicroMod Logo


Before getting started, be sure to check out our What is GPS RTK? tutorial and if you're not familiary with u-center, have a look at our Getting Started with U-Center as well as these related tutorials:

I2C

An introduction to I2C, one of the main embedded communications protocols in use today.

Serial Basic Hookup Guide

Get connected quickly with this Serial to USB adapter.

What is GPS RTK?

Learn about the latest generation of GPS and GNSS receivers to get 14mm positional accuracy!

Getting Started with U-Center for u-blox

Learn the tips and tricks to use the u-blox software tool to configure your GPS receiver.

This tutorial is based around the guide for the SparkFun GPS-RTK2 Board - ZED-F9P so you may want to check out these tutorials for more information on GPS-RTK:

GPS-RTK Hookup Guide

September 13, 2018
Find out where you are! Use this easy hook-up guide to get up and running with the SparkFun high precision GPS-RTK NEO-M8P-2 breakout board.

GPS-RTK2 Hookup Guide

January 14, 2019
Get precision down to the diameter of a dime with the new ZED-F9P from u-blox.

Hardware Overview

Let's take a closer look at the ZED-F9P module and other hardware on this Function Board.

ZED-F9P GNSS Module

The ZED-F9P is a high-precision GNSS module from u-blox capable of up to millimeter X, Y & Z positional accuracy.

Image highlighting the ZED-F9P module.

The ZED-F9P with a full RTK lock along with RTCM data streaming to the module can achieve 10mm 3D positional accuracy. Depending on the constellation the module achieves a lock in ~25 seconds from a cold start and 2 seconds from both a hot start and aided start. For a complete overview of the module, refer to the ZED-F9P datasheet.

One of the key differentiators between the ZED-F9P and almost all other low-cost RTK solutions is the ZED-F9P is capable of receiving both L1 and L2 bands.

L1 and L2 GNSS reception on the ZED-F9P

The module can act as either a rover to receive GNNS location data and RTCM correction data or a base station to send RTCM correction data to another device. For complete information on how to configure the ZED-F9P as a base station or rover, refer to the u-blox Integration Manual or check out this tutorial.

Communication Interfaces

This Function Board routes the ZED-F9P's USB interface to a USB-C connector on the top of the board. The SPI, I2C and primary serial interfaces are routed to the MicroMod M.2 connector through an isolation circuit.

Image highlighting the USB-C and MicroMod connections.

The board configures the ZED-F9P to communicate via I2C and Serial by default. Adjusting the DSEL solder jumper switches the communication interface to SPI.

The USB-C connector allows direct communication to the ZED-F9P UART interface but does not provide power to the module or other parts of the MicroMod assembly by default. To use this connector for power, adjust the USB PWR EN jumper. Read on to the Solder Jumpers section for more information.

Antenna

The board routes the ZED-F9P antenna connection to a u.Fl connector for an external antenna connection. Most of the recommended antennas use a SMA-type connector so an adapter like this is most likely needed.

Image highlighting the u.FL connector

The Function Board also includes a RF/antenna supervision circuit to monitor and control the active antenna connection. The supervision circuit protects the ZED-F9P from a short circuit on the antenna connection and monitors the antenna connection to detect a connected antenna or open circuit. By default the Function Board disables this circuit through the SUP solder jumper. Read on to the Solder Jumpers section for more information on using this jumper and refer to section 4.3.4 of the ZED-F9P Integration Manual for more information on this circuit and how to poll the status using UBX messages.

Backup Battery

The backup battery on the board has a 1.5mAh capacity to maintain settings and other low-power functionality to the ZED-F9P when the module is not fully powered.

Image highlighting the backup battery circuit.

PTH Connections

Along with the secondary serial bus, the Function Board routes several other ZED-F9P pins to plated through-hole (PTH) connecitons.

Image highlighting the PTH connections.

The list below outlines the labels and functionality of the PTH connections on the Function Board:

  • PPS - The board translates the Pulse-Per-Second (PPS) output to a differential output routed to a pair of PTHs along with matching ground PTHs.
  • RX2/TX2 - The ZED-F9P's secondary UART (RX2/TX2) along with a ground PTH.
  • Reset - ZED-F9P reset pin.
  • EXTINT - ZED-F9P external interrupt pin.
  • SB - ZED-F9P SafeBoot pin.
  • GND - Several Ground PTHs if needed.

LEDs

The GNSS Function Board - ZED-F9P has three LEDs labeled: PWR, PPS and RTK.

Image highlighting the LEDs.

  • PWR - Indicates when the ZED-F9P is powered.
  • PPS - Tied to the Pulse Per Second pin and acts as a visual indicator to the ZED-F9P pulse per second signal.
  • RTK - Indicates the status of the RTK lock.

Solder Jumpers

If you have never worked with solder jumpers and PCB traces before or would like a quick refresher, check out our How to Work with Solder Jumpers and PCB Traces tutorial for detailed instructions and tips.

This board has nine solder jumpers. The table below outlines each jumper's label, default state, function and notes regarding their use:

Image highlighting the solder jumpers.
Having trouble seeing the details in the photo? Click on it for a larger view.

Label Default State Function Notes
USBPWREN OPEN Enables USB power to ZED-F9P. Close to use the USB-C connector on the Function Board to power the ZED-F9P.
SHLD CLOSED USB-C shield control. Open to disconnect the USB-C shield pin to the ground plane.
SUP Disable Antenna supervisor circuit control. Disables the antenna supervisor circuit by default. Switch to EN side to enable the circuit.
DSEL ZED-F9P interface selection. I2C/Serial Three pad jumper controls which communication interface the ZED-F9P uses. Can be set to I2C/Serial (Default) or SPI.
I2C CLOSED I2C pull up resistors Three-way jumper pulling the SDA and SCL lines to 3.3V through a pair of 2.2kΩ resistors. Sever both traces to disable the pull up resistors.
WP EEPROM Write Protection OPEN Close to clarification needed write protection on the EEPROM IC.
PWR Power LED control. CLOSED Enables the ZED-F9P power indicator LED. Open to disable the LED.
PPS PPS LED control. CLOSED Enables the ZED-F9P pulse per second LED. Open to disable the LED.
RTK RTK LED control. CLOSED Enables the ZED-F9P RTK lock indicator LED. Open to disable the LED.

MicroMod Pinout

This Function Board uses the following pins on a connected Processor Board:

  • 3.3V & VCC
  • Power enable
  • SPI - ZED-F9P SPI
  • I2C - ZED-F9P I2C and EEPROM
  • UART RX1/TX1 (Slot 0) / UART RX2/TX2 (Slot 1) - ZED-F9P UART1
  • CS0 (Slot 0) / CS1 (Slot 1) - ZED-F9P Chip Select
  • D0 (Slot 0) / D1 (Slot 1) - ZED-F9P TX Ready
  • PWM0 (Slot 0) / PWM1 (Slot 1) - ZED-F9P Pulse-Per-Second
  • G0 (Slot 0) / G5 (Slot 1) - ZED-F9P Reset
  • G1 (Slot 0) / G6 (Slot 1) - External Interrupt
  • G2 (Slot 0) / G7 (Slot 1) - RTK Status
  • G3 (Slot 0) / G8 (Slot 1) - Geofence Status
Note: As covered previously, the ZED-F9P uses the same pins for UART/I2C (Default) and SPI depending on the state of the interface select (D_SEL) pin. The Function Board routes these interfaces to the labeled pins on the MicroMod M.2 connector through separate quad bilateral switches that are enabled/disabled depending on the state of the D_SEL pin controlled by the D_SEL solder jumper.

For the complete MicroMod Pinout and pins used by this function board, take a look at the tables below:

AUDIO UART GPIO/BUS I2C SDIO SPI0 Dedicated
Function Bottom
Pin
   Top   
Pin
Function
(Not Connected) 75 GND
3.3V 74 73 G5 / BUS5
RTC_3V_BATT 72 71 G6 / BUS6
SPI_CS1# SDIO_DATA3 (I/O) 70 69 G7 / BUS7
SDIO_DATA2 (I/O) 68 67 G8
SDIO_DATA1 (I/O) 66 65 G9 ADC_D- CAM_HSYNC
SPI_CIPO1 SDIO_DATA0 (I/O) 64 63 G10 ADC_D+ CAM_VSYNC
SPI COPI1 SDIO_CMD (I/O) 62 61 SPI_CIPO (I)
SPI SCK1 SDIO_SCK (O) 60 59 SPI_COPI (O) LED_DAT
AUD_MCLK (O) 58 57 SPI_SCK (O) LED_CLK
CAM_MCLK PCM_OUT I2S_OUT AUD_OUT 56 55 SPI_CS#
CAM_PCLK PCM_IN I2S_IN AUD_IN 54 53 I2C_SCL1 (I/O)
PDM_DATA PCM_SYNC I2S_WS AUD_LRCLK 52 51 I2C_SDA1 (I/O)
PDM_CLK PCM_CLK I2S_SCK AUD_BCLK 50 49 BATT_VIN / 3 (I - ADC) (0 to 3.3V)
G4 / BUS4 48 47 PWM1
G3 / BUS3 46 45 GND
G2 / BUS2 44 43 CAN_TX
G1 / BUS1 42 41 CAN_RX
G0 / BUS0 40 39 GND
A1 38 37 USBHOST_D-
GND 36 35 USBHOST_D+
A0 34 33 GND
PWM0 32 31 Module Key
Module Key 30 29 Module Key
Module Key 28 27 Module Key
Module Key 26 25 Module Key
Module Key 24 23 SWDIO
UART_TX2 (O) 22 21 SWDCK
UART_RX2 (I) 20 19 UART_RX1 (I)
CAM_TRIG D1 18 17 UART_TX1 (0)
I2C_INT# 16 15 UART_CTS1 (I)
I2C_SCL (I/0) 14 13 UART_RTS1 (O)
I2C_SDA (I/0) 12 11 BOOT (I - Open Drain)
D0 10 9 USB_VIN
SWO G11 8 7 GND
RESET# (I - Open Drain) 6 5 USB_D-
3.3V_EN 4 3 USB_D+
3.3V 2 1 GND
Description Function Bottom
Pin
   Top   
Pin
Function Description
(Not Connected) 75 GND
- 74 73 3.3V Power Supply: 3.3-6V
- 72 71 Power EN Power Enable
- 70 69 -
- 66 65 -
- 64 63 -
- 62 61 -
- 60 59 GEO_STAT ZED-F9P Geofence Status Signal
- 58 57 RTK_STAT ZED-F9P RTK Lock Status Signal
- 56 55 EXTINT ZED-F9P External Interrupt
- 54 53 RESET ZED-F9P Reset
- 52 51 PPS ZED-F9P Pulse-Per-Second Signal
- 50 49 CS ZED-F9P Chip Select
- 48 47 TX_READY ZED-F9P UART TX Ready Signal
- 46 45 GND
- 44 43 -
- 42 41 -
Write protection pin for the EEPROM. Pull low to enable. EEPROM_WP 40 39 GND
- 38 37 -
EEPROM I2C address configuration. EEPROM_A0 36 35 -
EEPROM I2C address configuration. EEPROM_A1 34 33 GND
EEPROM I2C address configuration. EEPROM_A2 32 31 Module Key
Module Key 30 29 Module Key
Module Key 28 27 Module Key
Module Key 26 25 Module Key
Module Key 24 23 -
- 22 21 I2C_SCL I2C - Clock Signal
- 20 19 I2C_SDA I2C - Data Signal
- 18 17 -
- 16 15 RX ZED RX
- 14 13 TX ZED TX
- 12 11 -
- 10 9 -
- 8 7 POCI SPI Peripheral Output/Controller Input.
- 6 5 PICO SPI Peripheral Input/Controller Output.
- 4 3 SCK SPI Clock Signal
- 2 1 GND
Signal Group Signal I/O Description Voltage
Power 3.3V I 3.3V Source 3.3V
GND Return current path 0V
USB_VIN I USB VIN compliant to USB 2.0 specification. Connect to pins on processor board that require 5V for USB functionality 4.8-5.2V
RTC_3V_BATT I 3V provided by external coin cell or mini battery. Max draw=100μA. Connect to pins maintaining an RTC during power loss. Can be left NC. 3V
3.3V_EN O Controls the carrier board's main voltage regulator. Voltage above 1V will enable 3.3V power path. 3.3V
BATT_VIN/3 I Carrier board raw voltage over 3. 1/3 resistor divider is implemented on carrier board. Amplify the analog signal as needed for full 0-3.3V range 3.3V
Reset Reset I Input to processor. Open drain with pullup on processor board. Pulling low resets processor. 3.3V
Boot I Input to processor. Open drain with pullup on processor board. Pulling low puts processor into special boot mode. Can be left NC. 3.3V
USB USB_D± I/O USB Data ±. Differential serial data interface compliant to USB 2.0 specification. If UART is required for programming, USB± must be routed to a USB-to-serial conversion IC on the processor board.
USB Host USBHOST_D± I/O For processors that support USB Host Mode. USB Data±. Differential serial data interface compliant to USB 2.0 specification. Can be left NC.
CAN CAN_RX I CAN Bus receive data. 3.3V
CAN_TX O CAN Bus transmit data. 3.3V
UART UART_RX1 I UART receive data. 3.3V
UART_TX1 O UART transmit data. 3.3V
UART_RTS1 O UART ready to send. 3.3V
UART_CTS1 I UART clear to send. 3.3V
UART_RX2 I 2nd UART receive data. 3.3V
UART_TX2 O 2nd UART transmit data. 3.3V
I2C I2C_SCL I/O I2C clock. Open drain with pullup on carrier board. 3.3V
I2C_SDA I/O I2C data. Open drain with pullup on carrier board 3.3V
I2C_INT# I Interrupt notification from carrier board to processor. Open drain with pullup on carrier board. Active LOW 3.3V
I2C_SCL1 I/O 2nd I2C clock. Open drain with pullup on carrier board. 3.3V
I2C_SDA1 I/O 2nd I2C data. Open drain with pullup on carrier board. 3.3V
SPI SPI_PICO O SPI Peripheral Input/Controller Output. 3.3V
SPI_POCI I SPI Peripheral Output/Controller Input. 3.3V
SPI_SCK O SPI Clock. 3.3V
SPI_CS# O SPI Chip Select. Active LOW. Can be routed to GPIO if hardware CS is unused. 3.3V
SPI/SDIO SPI_SCK1/SDIO_CLK O 2nd SPI Clock. Secondary use is SDIO Clock. 3.3V
SPI_PICO1/SDIO_CMD I/O 2nd SPI Peripheral Input/Controller Output. Secondary use is SDIO command interface. 3.3V
SPI_POCI1/SDIO_DATA0 I/O 2nd SPI Controller Output/Peripheral Input. Secondary use is SDIO data exchange bit 0. 3.3V
SDIO_DATA1 I/O SDIO data exchange bit 1. 3.3V
SDIO_DATA2 I/O SDIO data exchange bit 2. 3.3V
SPI_CS1/SDIO_DATA3 I/O 2nd SPI Chip Select. Secondary use is SDIO data exchange bit 3. 3.3V
Audio AUD_MCLK O Audio master clock. 3.3V
AUD_OUT/PCM_OUT/I2S_OUT/CAM_MCLK O Audio data output. PCM synchronous data output. I2S serial data out. Camera master clock. 3.3V
AUD_IN/PCM_IN/I2S_IN/CAM_PCLK I Audio data input. PCM syncrhonous data input. I2S serial data in. Camera periphperal clock. 3.3V
AUD_LRCLK/PCM_SYNC/I2S_WS/PDM_DATA I/O Audio left/right clock. PCM syncrhonous data SYNC. I2S word select. PDM data. 3.3V
AUD_BCLK/PCM_CLK/I2S_CLK/PDM_CLK O Audio bit clock. PCM clock. I2S continuous serial clock. PDM clock. 3.3V
SWD SWDIO I/O Serial Wire Debug I/O. Connect if processor board supports SWD. Can be left NC. 3.3V
SWDCK I Serial Wire Debug clock. Connect if processor board supports SWD. Can be left NC. 3.3V
ADC A0 I Analog to digital converter 0. Amplify the analog signal as needed to enable full 0-3.3V range. 3.3V
A1 I Analog to digital converter 1. Amplify the analog signal as needed to enable full 0-3.3V range. 3.3V
PWM PWM0 O Pulse width modulated output 0. 3.3V
PWM1 O Pulse width modulated output 1. 3.3V
Digital D0 I/O General digital input/output pin. 3.3V
D1/CAM_TRIG I/O General digital input/output pin. Camera trigger. 3.3V
General/Bus G0/BUS0 I/O General purpose pins. Any unused processor pins should be assigned to Gx with ADC + PWM capable pins given priority (0, 1, 2, etc.) positions. The intent is to guarantee PWM, ADC and Digital Pin functionality on respective ADC/PWM/Digital pins. Gx pins do not guarantee ADC/PWM function. Alternative use is pins can support a fast read/write 8-bit or 4-bit wide bus. 3.3V
G1/BUS1 I/O 3.3V
G2/BUS2 I/O 3.3V
G3/BUS3 I/O 3.3V
G4/BUS4 I/O 3.3V
G5/BUS5 I/O 3.3V
G6/BUS6 I/O 3.3V
G7/BUS7 I/O 3.3V
G8 I/O General purpose pin 3.3V
G9/ADC_D-/CAM_HSYNC I/O Differential ADC input if available. Camera horizontal sync. 3.3V
G10/ADC_D+/CAM_VSYNC I/O Differential ADC input if available. Camera vertical sync. 3.3V
G11/SWO I/O General purpose pin. Serial Wire Output 3.3V

Board Dimensions

The board matches the MicroMod Function Board design specifications and measures 2.56" x 1.48" (65.02mm x 37.69mm) and the USB-C connector protrudes roughly 0.067" (1.70mm) from the edge of the board.

Image of board dimensions

Hardware Assembly

If you're not familiar with assembling boards using the MicroMod connection system, head over to the MicroMod Main Board Hookup Guide for information on inserting and securing your MicroMod Processor and Function Boards to the Main Board:

MicroMod Main Board Hookup Guide

November 11, 2021
The MicroMod Main Board - Single and Double are specialized carrier boards that allow you to interface a Processor Board with a Function Board(s). The modular system allows you to add an additional feature(s) to a Processor Board with the help of a Function Board(s). In this tutorial, we will focus on the basic functionality of the Main Board - Single and Main Board - Double.

Antenna Connection

The antenna connection on this Function Board uses a u.Fl connector so an adapter like this is most likely needed. For tips on how to properly use a u.Fl connector, this tutorial can help.

Completed Assembly

With the Function and Processor Boards installed on a Main Board and the antenna and USB-C cables plugged in, your completed MicroMod assembly should look similar to the photo below:

Image of completed MicroMod assembly with GNSS antenna connected.

With the MicroMod assembly completed, we can move on to setting up the software and start getting location data from the ZED-F9P.

Software Installation

Note: This example assumes you are using the latest version of the Arduino IDE on your desktop. If this is your first time using Arduino, please review the following tutorials.

SparkFun u-blox Arduino Library

Note: This example assumes you are using the latest version of the Arduino IDE on your desktop. If this is your first time using Arduino, please review our tutorial on installing the Arduino IDE. If you have not previously installed an Arduino library, please check out our installation guide.

The SparkFun u-blox Arduino library enables the reading of all positional datums as well as sending binary UBX configuration commands over I2C. This is helpful for configuring advanced modules like the ZED-F9P but also the NEO-M8P-2, SAM-M8Q and any other u-blox module that use the u-blox binary protocol.

Note: We support two versions of the SparkFun u-blox GNSS library. Version 2 and Version 3. Version 3 uses the u-blox Configuration Interface (VALSET and VALGET) to configure the module, instead of the deprecated UBX-CFG messages. For modules like the F9 and M10, we recommend upgrading to Version 3. However, older modules like the M8 do not support the Configuration Interface. For those you will need to keep using Version 2 of the library. We will continue to support both.

The SparkFun u-blox Arduino library can be downloaded with the Arduino library manager by searching 'SparkFun u-blox GNSS v3' or you can grab the zip here from the GitHub repository to manually install.

This SparkFun u-blox library really focuses on I2C because it's faster than serial and supports daisy-chaining. The library also uses the UBX protocol because it requires far less overhead than NMEA parsing and does not have the precision limitations that NMEA has.

In the next section we'll look at the first example included with the library to verify everything is working properly with the GNNS Function Board - ZED-F9P.

u-center Installation

For those who prefer to communicate directly with the ZED-F9P through the USB-C connector on the Function Board, head over to this tutorial to get started with u-center from u-blox:

Getting Started with U-Center for u-blox

September 13, 2018
Learn the tips and tricks to use the u-blox software tool to configure your GPS receiver.

Pin Connection Table

The table below helps show which pins the Function Board connects to depending on the slot it is connected to on a Main Board (Note: The Single Main Board connection is Slot 0):

AUDIO UART GPIO/BUS I2C SDIO SPI0 Dedicated
Function Board
Pin Name
Main Board's
Processor Pin
Slot 0 Slot 1
VCC -
3.3V -
GND -
ZED_RX TX1 TX2
ZED_TX RX1 RX2
TX READY D0 D1
CS CS0 CS1
PPS PWM0 PWM1
RST G0 G5
INT G1 G6
RTK G2 G7
GEO G3 G8

Arduino Example

Example 1: Positional Accuracy

The first example in the SparkFun u-blox GNSS Arduino Library provides a quick test for position and accuracy. Navigate to the example by going to File > Examples > SparkFun u-blox GNSS v3 > ZED-F9P > Example1_GetPositionAccuracy.

Select your Board (in this case the SparkFun ESP32 MicroMod) and associated COM port. Upload the code and open the Arduino Serial Monitor with the baud set to 115200. Make sure the antenna has a clear view of the sky and give the ZED-F9P some time to get a satellite lock. Once the module gets a satellite lock the coordinates and accuracy should start to print out in the serial monitor window.

More Examples!

Now that you got it up and running, check out the other examples located in the ZED-F9P folder!

In order to get the most out of the ZED-F9P, you will need an RTCM correction source. Depending on your choice of Processor or other items in your setup, you may need a second ZED-F9P for a correction source. The following project tutorials guide you through setting up the ZED-F9P as a reference station or rover.

How to Build a DIY GNSS Reference Station

October 15, 2020
Learn how to affix a GNSS antenna, use PPP to get its ECEF coordinates and then broadcast your own RTCM data over the internet and cellular using NTRIP to increase rover reception to 10km!

Setting up a Rover Base RTK System

October 14, 2020
Getting GNSS RTCM correction data from a base to a rover is easy with a serial telemetry radio! We'll show you how to get your high precision RTK GNSS system setup and running.

Troubleshooting

u.Fl Tips

Unplugging the u.Fl adapter from the connector on the Function Board is tricky and improper removal can damage the connector or the board. For tips on using the u.Fl connector, check out this tutorial:

Three Quick Tips About Using U.FL

December 28, 2018
Quick tips regarding how to connect, protect, and disconnect U.FL connectors.

Position Lock Tips

Depending on your antenna choice and setup, you may experience issues getting your ZED-F9P to achieve a 3D lock. If you run into issues getting a lock, make sure the antenna has a clear view of the sky away from large objects such as buildings that may block the antenna view.

General Troubleshooting

Resources and Going Further

That's all for this tutorial. By now you should be able to start recording positional data with your completed MicroMod Main Board assembly using the GNSS Function Board - ZED-F9P. For more information, check out the following resources:

MicroMod GNSS Function Board Documentation:

ZED-F9P Documentation:

MicroMod Documentation:

Looking for inspiration for a GNSS-RTK project? The following tutorials can help you get started:

Building an Autonomous Vehicle: The Batmobile

Documenting a six-month project to race autonomous Power Wheels at the SparkFun Autonomous Vehicle Competition (AVC) in 2016.

What is GPS RTK?

Learn about the latest generation of GPS and GNSS receivers to get 14mm positional accuracy!

Setting up a Rover Base RTK System

Getting GNSS RTCM correction data from a base to a rover is easy with a serial telemetry radio! We'll show you how to get your high precision RTK GNSS system setup and running.

How to Build a DIY GNSS Reference Station

Learn how to affix a GNSS antenna, use PPP to get its ECEF coordinates and then broadcast your own RTCM data over the internet and cellular using NTRIP to increase rover reception to 10km!