MicroMod Ethernet Function Board - W5500 Hookup Guide

≡ Pages
Contributors: El Duderino

Software Installation

Note: The Ethernet Arduino example assumes you are using the latest version of the Arduino IDE on your desktop. If this is your first time using Arduino, please review the following tutorials.

Processor Arduino Board Definitions and Driver

Make sure you go through the Hookup Guide for your chosen Processor Board to install the Arduino board definitions and any necessary drivers:

MicroMod ESP32 Processor Board Hookup Guide

October 21, 2020
A short hookup guide to get started with the SparkFun MicroMod ESP32 Processor Board.

MicroMod STM32 Processor Hookup Guide

May 13, 2021
Get started with the MicroMod Ecosystem and the STM32 Processor Board!

MicroMod Teensy Processor Hookup Guide

July 1, 2021
Add the processing power and versatility of the Teensy to your MicroMod project following this guide for the SparkFun MicroMod Teensy Processor.
Note on Artemis and nRF52840 Processors: Currently the Artemis and nRF52840 do not have built in Ethernet libraries in their Arduino cores. An external Arduino Ethernet library may work but at this time Ethernet is not supported on those Processors. We will update the tutorial in the future if Ethernet support is added to these cores.

Main Board Example - Pin Connection Table

The table below helps show what pins the Function Board connects to depending on the slot it is connected to on a Main Board (Note: The Single Main Board connection is Slot 0):

AUDIO UART GPIO/BUS I2C SDIO SPI0 Dedicated
Function Board
Pin Name
I/O
Direction
Main Board's
Processor Pin
Slot 0 Slot 1
VCC Input -
3.3V Input -
GND - -
ETH_INT D0 D1
CS CS0 CS1
ETH_RST PWM0 PWM1