MicroMod Ethernet Function Board - W5500 Hookup Guide

≡ Pages
Contributors: El Duderino

Arduino Example

Now that our MicroMod system is fully assembled, we'll use a slightly modified version of the "Ethernet - Web Client" example included with Arduino to make sure everything is connected and working properly. This modified version simply updates the options for the SPI Chip Select pin to match those used on supported MicroMod Processor Boards:

language:c
void setup() {
  //Ethernet.init(CS); //SAMD51
  Ethernet.init(10); //Teensy
  //Ethernet.init(5); //ESP32
  //Ethernet.init(A4); //STM32    
Note: The code defaults to use the CS pin used with the Function Board connected in Slot 0. If the board is in Slot 1, switch to the CS1 pin on your Processor.

Open the Arduino IDE and either copy the code below or navigate to the example by going to File > Examples > Ethernet > Web Client. Reminder, if you open the default example in Arduino, make sure to set the correct Chip Select pin for the Processor Board used as listed above. Upload the code and open the serial monitor with the baud set to 115200 and you should see the example initialize the W5500 and ping Google.com.

language:c
/*
  Web client
 This sketch connects to a website (http://www.google.com)
 using an Arduino Wiznet Ethernet shield.
 Circuit:
 * Ethernet shield attached to pins 10, 11, 12, 13
 created 18 Dec 2009
 by David A. Mellis
 modified 9 Apr 2012
 by Tom Igoe, based on work by Adrian McEwen
 */

#include <SPI.h>
#include <Ethernet.h>

// Enter a MAC address for your controller below.
// Newer Ethernet shields have a MAC address printed on a sticker on the shield
byte mac[] = { 0xDE, 0xAD, 0xBE, 0xEF, 0xFE, 0xED };

// if you don't want to use DNS (and reduce your sketch size)
// use the numeric IP instead of the name for the server:
//IPAddress server(74,125,232,128);  // numeric IP for Google (no DNS)
char server[] = "www.google.com";    // name address for Google (using DNS)

// Set the static IP address to use if the DHCP fails to assign
IPAddress ip(192, 168, 0, 177);
IPAddress myDns(192, 168, 0, 1);

// Initialize the Ethernet client library
// with the IP address and port of the server
// that you want to connect to (port 80 is default for HTTP):
EthernetClient client;

// Variables to measure the speed
unsigned long beginMicros, endMicros;
unsigned long byteCount = 0;
bool printWebData = false;  // set to false for better speed measurement

void setup() {
  //Ethernet.init(CS); //SAMD51
  Ethernet.init(10); //Teensy
  //Ethernet.init(5); //ESP32
  //Ethernet.init(A4); //STM32

  Serial.begin(115200);

  delay(4000);

  // start the Ethernet connection:
  Serial.println("Initialize Ethernet with DHCP:");
  if (Ethernet.begin(mac) == 0) {
    Serial.println("Failed to configure Ethernet using DHCP");
    // Check for Ethernet hardware present
    if (Ethernet.hardwareStatus() == EthernetNoHardware) {
      Serial.println("Ethernet shield was not found.  Sorry, can't run without hardware. :(");
      while (true) {
        delay(1000);
        Serial.println("Not detected");
        delay(1); // do nothing, no point running without Ethernet hardware
      }
    }
    if (Ethernet.linkStatus() == LinkOFF) {
      Serial.println("Ethernet cable is not connected.");
    }
    // try to congifure using IP address instead of DHCP:
    Ethernet.begin(mac, ip, myDns);
  } else {
    Serial.print("  DHCP assigned IP ");
    Serial.println(Ethernet.localIP());
  }
  // give the Ethernet shield a second to initialize:
  delay(1000);
  Serial.print("connecting to ");
  Serial.print(server);
  Serial.println("...");

  // if you get a connection, report back via serial:
  if (client.connect(server, 80)) {
    Serial.print("connected to ");
    Serial.println(client.remoteIP());
    // Make a HTTP request:
    client.println("GET /search?q=arduino HTTP/1.1");
    client.println("Host: www.google.com");
    client.println("Connection: close");
    client.println();
  } else {
    // if you didn't get a connection to the server:
    Serial.println("connection failed");
  }
  beginMicros = micros();
}

void loop() {
  // if there are incoming bytes available
  // from the server, read them and print them:
  int len = client.available();
  if (len > 0) {
//    byte buffer[80];
    byte buffer[512 * 4];
    if (len > sizeof(buffer)) len = sizeof(buffer);
    client.read(buffer, len);
    if (printWebData) {
      Serial.write(buffer, len); // show in the serial monitor (slows some boards)
    }
    byteCount = byteCount + len;
  }

  // if the server's disconnected, stop the client:
  if (!client.connected()) {
    endMicros = micros();
    Serial.println();
    Serial.println("disconnecting.");
    client.stop();
    Serial.print("Received ");
    Serial.print(byteCount);
    Serial.print(" bytes in ");
    float seconds = (float)(endMicros - beginMicros) / 1000000.0;
    Serial.print(seconds, 4);
    float rate = (float)byteCount / seconds / 1000.0;
    Serial.print(", rate = ");
    Serial.print(rate);
    Serial.print(" kbytes/second");
    Serial.println();

    // do nothing forevermore:
    while (true) {
      delay(1);
    }
  }
}