MicroMod ESP32 Processor Board Hookup Guide

≡ Pages
Contributors: Alex the Giant, Ell C

Troubleshooting

With the MicroMod Processors, you can change out the processors with little to no changes in the code. But because each processor board's architecture is different, the way communication protocols are initialized might be a little bit different. For the ESP32 Processor, the two main protocols are the Universal Asynchronous Receiver Transmitter (UART), aka Serial, and I2C, aka Wire.

Secondary Serial/UART Initialization Tips

The UART is initialized with the begin function as:

void begin(unsigned long baud, uint32_t config, int8_t rxPin, int8_t txPin, bool invert, unsigned long timeout_ms)

The primary UART works like any other Arduino board being able to initialize and send messages back to your computer over the USB cable using using Serial.begin(115200) for a baud rate of 115200 as an example. If you wanted to communicate at the same 115200 baud rate on the secondary UART you would initialize Serial1 as:

Serial1.begin(115200, SERIAL_8N1, RX1,TX1);

Or if you want to use the GPIO pin numbers instead, it would be:

Serial1.begin(115200, SERIAL_8N1, 16, 17);

Secondary I2C Initialization Tips

The Wire bus is initialized with the begin function as:

bool begin(int sda, int scl, uint32_t frequency);  // returns true, if successful init of i2c bus

With the primary Wire bus, these pins use the default SCL and SDA pins connected to GPIO pins 22 and 21 and can be initialized by simply calling Wire.begin(). If you plan on using the secondary Wire bus, you need to provide the pins, and possibly the desired frequnecy if the default 400kHz is too fast. For most applications though you can use:

Wire1.begin(SDA1, SCL1);

Or if you wanted to use the GPIO pin numbers, it would be:

Wire1.begin(26, 25);