micro:bit Breakout Board Hookup Guide

≡ Pages
Contributors: Shawn Hymel, Ell C

Resources and Going Further

With the micro:bit breakout board, you can start introducing more sensors, lights, and motors into your project! For more information, check out these resources:

Need some inspiration for your next project? Check out some of these related tutorials:

MPU-9150 Hookup Guide

A basic guide to get started with the MPU-9150 9 Degrees of Freedom Breakout.

SparkFun Inventor's Kit Experiment Guide - v4.0

The SparkFun Inventor's Kit (SIK) Experiment Guide contains all of the information needed to build all five projects, encompassing 16 circuits, in the latest version of the kit, v4.0a.

Air Velocity Sensor Breakout - FS3000 Hookup Guide

Get started with the Air Velocity Sensor Breakout - FS3000!

SparkFun Indoor Air Quality Sensor - ENS160 (Qwiic) Hookup Guide

Is your air safe? Check your eCO2, TVOC, and AQI levels with the new SparkFun Indoor Air Quality Sensor - ENS160!

Qwiic Accelerometer (MMA8452Q) Hookup Guide

Freescale’s MMA8452Q is a smart, low-power, three-axis, capacitive micro-machined accelerometer with 12-bits of resolution. It’s perfect for any project that needs to sense orientation or motion. We’ve taken that accelerometer and stuck it on a Qwiic-Enabled breakout board to make interfacing with the tiny, QFN package a bit easier.

Hookup Guide for the Qwiic Motor Driver

Drive things "qwiic"-ly with the SparkFun Qwiic Motor Driver!

SparkFun Qwiic Shield for Teensy Hookup Guide

A short guide for assembling and using the SparkFun Qwiic Shield for Teensy and Qwiic Shield for Teensy Extended.

smôl Header Hookup Guide

Small in size, small on current draw. It's a smôl world! This guide will get you up and running with the smôl Header.