LuMini Ring Hookup Guide
Contributors:
Englandsaurus
Resources & Going Further
Now that you've successfully got your LuMini Ring up and running, it's time to incorporate it into your own project! For more information about the LuMini Ring, check out the links below.
Lumini Ring 3 Inch
Lumini Ring 2 Inch
Lumini Ring 1 Inch
- Datasheet - APA102 (PDF)
- SMD Soldering Tips and Tricks
- GitHub FastLED Arduino Library
- GitHub Code -- Example used in this tutorial can be found in the LuMini Ring 3 Inch Repo
- SFE Product Showcase
Looking for a different way of controlling the LuMini Rings? Check out the LuMini Drive to program the APA102's in Circuit Python.
LumiDrive Hookup Guide
The LumiDrive LED Driver is SparkFun’s foray into all things Python on micro-controllers. With the SparkFun LumiDrive you will be able to control and personalize a whole strand of APA102s directly from the board itself.
Need some inspiration for your next project? Check out some of these related tutorials:
Let It Glow Holiday Cards
Craft a glowing card for friends and family this holiday season with paper circuits - no soldering required!
Hackers in Residence: The Sound Visualizer Pt. 2
An addition to a previous project, this time using a PC and a custom Java app to create your own music visualizer using a RGB LED matrix.
LED Cloud-Connected Cloud
Make an RGB colored cloud light! You can also control it from your phone, or hook up to the weather!
Experiment Guide for the Johnny-Five Inventor's Kit
Use the Tessel 2 and the Johnny Five Inventors kit to explore the world of JavaScript enabled hardware through 14 awesome experiments!
Or check out these blog post: