LuMini Ring Hookup Guide

≡ Pages
Contributors: Englandsaurus

Hardware Overview

I/O Pins

The LuMini rings are powered and controlled using a few pads on the back of each board. Each board has a set of pads for 5V and ground, a set of pads for data and clock input, and a set of pads for data and clock output. These pads are outlined in the below image.

I/O Pads

I/O Pads

Decoupling Capacitor Pads

In larger installations you may need to add a decoupling capacitor between power and ground to prevent voltage dips when turning on a whole bunch of LED's simultaneously. The spot to add this optional capacitor is outlined below.

Capacitor Pads

Capacitor Pads

We'd recommend the surface mount 4.7 µF capacitor that is shown below. If you've never done surface mount soldering before, this part might be a little tricky, but check out our SMD tips and tricks on doing just that.

Capacitor 4.7uF - SMD (Strip of 10)

COM-15169
Retired

LED Numbers

Looking at the back of each ring, you'll also see some numbers. Since the ring acts like a string of LEDs, these numbers correspond to the LED number in the string. Note that, like the led array, we index at LED 0, so calling leds[5] will correspond to the LED on the opposite side of the 5 labeling.

LED Numbers

LED Numbers