Interactive Smart Mirror

≡ Pages
Contributors: Shawn Hymel

Other Dependencies

With the UPM modules installed, we can work on writing the actual code. That does mean we need to install a few more dependencies, though.

Other Node Libraries

We need one more library for our code. Luckily, we can install it through npm:

cd ~
npm install xml2js

NTP

We will want our Edison system time to be up-to-date. To do that, we will rely on an NTP service to regularly poll an Internet-connected server for the most accurate time.

Open the package manager file with:

vi /etc/opkg/base-feeds.conf

Press 'i' to start typing, and enter the following:

src/gz all http://repo.opkg.net/edison/repo/all
src/gz edison http://repo.opkg.net/edison/repo/edison
src/gz core2-32 http://repo.opkg.net/edison/repo/core2-32

Press 'esc', and enter ':wq' to save and exit. Update the package manager, and install the NTP client:

opkg update
opkg install ntp

Configure the NTP client:

vi /etc/ntp.conf

Find the line that says "server 127.127.1.0" and change it to (press 'i' to edit):

server pool.ntp.org

Your file should look like this:

Configure NTP client

Save and exit ('esc' and ':wq'). Next, we want to adjust our system's local time to our timezone. Since I am in Mountain Standard Time, I'm going to use MST. We do this by creating a symbolic link /etc/localtime that points to the timezone we want in /usr/share/zoneinfo/ (note that I'm using MST for my timezone).

rm /etc/localtime
ln -s /usr/share/zoneinfo/MST /etc/localtime

When we're done, reboot:

reboot

You can check your timezone by entering the command:

date

This should print out the date, time, and timezone.

Checking timezone in Linux

Configure OpenWeatherMap

We will be using OpenWeatherMap for our weather data, as it offers good hourly forecast data. In your browser, navigate to OpenWeatherMap's sign up page. Enter your credentials to make an account. Once you have logged in, scroll down on your profile page, and copy down your API key.

OpenWeatherMap API key

Find Your Location

We also need to find our location so we can pass that to OpenWeatherMap. Open up Google Maps, and place a marker at the location where you want to get weather data (left-click on the map). A pop-up note will appear with the latitude and longitude data.

Using Google Maps to get latitude and longitude

Copy down those two numbers as well. We'll need them.