How to Install FTDI Drivers

≡ Pages
Contributors: Paul Smith

Mac

Notice: The screen shots in this tutorial are from OS X 10.6. The process should be very similar, if not exactly the same, for other versions of Mac OS X. If you are on OS X 10.10 Yosemite, follow along to install the drivers. If you need to install drivers on Yosemite, please visit the bottom of this section. Most people will be using the VCP drivers and not the D2XX drivers.
Note for Educators: You will most likely need to obtain administrative privileges from your network or IT administrator in order to install these drivers.
  1. Most of the time, when you install Arduino on Mac OS X, the drivers are installed automatically. However, if there was a problem with the installation and you don't see any options that include 'usbserial' under the 'Tools -> Serial Port' menu, then you will need to install the drivers. You may also need to install the full FTDI drivers if you are running OSX 10.10 or later. The factory drivers are not complete.

    No USB devices

  2. a.) OS X 10.9 (Mavericks) or above: Download this driver. Locate the file FTDIUSBSerialDriver_v2_4.2.dmg file that was downloaded to your computer, and double click on it to open \ run it.

    You may need to visit FTDI’s VCP Drivers page for the latest download of the Mac OS X FTDI Driver. Click on the link for the "Mac OS X 10.9 and above" driver's version. The image below shows version 2.4.2 so you would need to click on **2.4.2* to download the latest driver. If there is an update to the drivers by FTDI, the version number will change but it should be in the same location on the table.

    Latest Mac FTDI Driveres

    b.) OS X 10.8 (Mountain Lion) or lower: Download this driver. Locate the file FTDIUSBSerialDriver_v2_2_18.dmg file that was downloaded to your computer, and double click on it to open \ run it.

    If you are using the driver for OS X 10.8 (Mountain Lion) or older, you will see two files. Open up the driver file that corresponds with your operating system. For most users, it will be the second file:

    Choose Correct OS version

  3. Continue through the installation, and wait for it to finish. Then click 'Close.'

    Continue Through Installation

  4. Now open the Arduino IDE. Under 'Tools -> Serial Port' you will now see a 'usbserial' option. Congratulations, you're all set!

Success


Troubleshooting: Unidentified Developer Error

On newer versions of OS X, when you double-click the install packages inside the FTDI disk image, you may be presented with a very Windows-esque type error about not being able to open the files because they are not from an identified developers. This is very similar to the unsigned driver issue in Windows 8.

alt text

Quick Fix

To get around this, simply right-click the package you want to install, or press CTRL + click, if you don't have a right-click. Then select open from the menu.

alt text

You will then be given another window asking if you are certain. Click Open, and proceed with the installation as stated above.

alt text

In-Depth Fix

For a more permanent fix, you can follow these instructions. **However, this method is not suggested as it leaves your computer vulnerable. **

Open your System Preferences.

alt text

Once open, click the Security & Privacy icon.

alt text

Under the General tab, you should see a section about allowing the running of downloaded applications from specific sources. In preveious version of OS X, the default was set to Anywhere. However, the defualt setting is now Mac App Store and identified developers.

alt text

To use the FTDI drivers, you'll need to set this back to Anywhere. First, you may need to click on the little lock icon and enter your admin password to make these changes.

Once unlocked, click the Anywhere option. Another obnoxious window may appear asking you if you're sure you want to allow this. Click Allow from Anywhere. Or, you can follow the directions in this window, if you don't want to make your Mac "less secure."

alt text

You should now be able to install the FTDI drivers.

alt text


Troubleshooting: FTDI Drivers and OS X Yosemite

With Mac OS 10.9 (Mavericks) and later, Apple has built their own version of the FTDI VCP driver into the operating system (AN134). However, there seems to be some conflict between drivers from FTDIchip.com and the ones inherent to Apple. Luckily, there is a solution to this problem, and it comes from FTDI directly.

Quick Fix

If you are trying to use the FTDI VCP Driver in your applications, it will not work due to a conflict between the VCP and D2XX drivers. In order to get around this, the Apple supplied Driver must be uninstalled. Plug in the FTDI device in question, and type the following command in a Terminal window:

sudo kextunload –b com.apple.driver.AppleUSBFTDI  <ret>

In-Depth Fix

If the above doesn't work, you may have better luck using this script from FTDI.

Clicking on this file will bring up the Script Editor on all Macs. The script can be run by clicking on the run icon (black triangle). Again, make sure your FTDI device is connected.

You can make this script into a clickable icon by exporting the script as an application. In the Script Editor, select Export… from the File pull down menu:

alt text

In the Export dialog, select Application as the File Format. You can choose any name for the application.

alt text

You should now have an automated Apple Script icon to use on your Mac. With the Apple supplied Drivers uninstalled, you may return to the top of this section and install the FTDI VCP Driver as needed. Repeat this process for any other FTDI devices you are using. You may need to repeat this every time you restart your computer.


Troubleshooting: No FTDI Driver Installed

If you receive this error, it means that the driver has been uninstalled already, and you will need to install the FTDI VCP Driver, as stated above.

alt text