How to Install FTDI Drivers

≡ Pages
Contributors: Paul Smith

Meet the FT232RL

The FT232RL is one of the more commonly used ICs used to convert USB signals to UART signals. This process is very handy in that it allows you communicate with and upload code to an Arduino or other microcontroller without the need for an external programmer. SparkFun carries a board called the FTDI Basic that conveniently breaks out the necessary pins on the FT232RL to perform these actions.

SparkFun FTDI

SparkFun's 5V FTDI Basic. Notice the IC--FT232RL.

There are a few different flavors of the FTDI Basic:

SparkFun FTDI Basic Breakout - 5V

DEV-09716
$17.50

SparkFun USB to Serial Breakout - FT232RL

BOB-12731
$22.95

SparkFun FT231X Breakout

BOB-13263
$14.95

SparkFun FTDI Starter Kit - 3.3V

KIT-18289
$15.95

If you are using a 5 volt device, you will need the 5 volt FTDI. If you have a 3.3 volt device, you guessed it, use a 3.3 volt FTDI. LilyPad boards all operate on 3.3V.

We also carry a complete breakout board for the FT232RL should you need access to more pins than the FTDI Basic provides.

SparkFun USB to Serial Breakout - FT232RL

BOB-12731
$22.95

Here is a list of some SparkFun products that require the use of an FTDI Basic, come with an FTDI Basic, or have an FT232RL chip on board:

There are also some legacy Arduino boards that use the FT232RL. The Arduino Diecimila and Duemilanove main boards along with the original Arduino Mega all use the FT232RL IC. If you have one of these older versions, you'll want to use the FDTI drivers as well. For a complete list of all Arduino boards, check out this page. Newer versions of Arduino boards, such as the Uno, use a different communication IC, and they will not be covered in this tutorial.

Now that you know why the FTDI Basic is important and what products it is used for, let's learn how to install the drivers.