Haptic Motor Driver Hook-Up Guide

≡ Pages
Contributors: LightningHawk

Introducing the Haptic Motor Driver

Ready to add some good vibes to your project? Look no further than the Haptic Motor Driver. This board breaks out Texas Instruments' DRV2605L haptic motor driver, which has some seriously cool features. Add meaningful feedback from your devices using the Haptic Motor Driver and an Arduino compatible device. This tutorial will get you up and running, or vibing, in no time with the I2C library for Arduino and example projects that give you the hardware setup and the code for various modes of operation.

SparkFun Haptic Motor Driver - DRV2605L

ROB-14538
$11.95

Features

  • Flexible Haptic and Vibration Driver for both ERM and LRA type motors
  • I2C Controlled Digital Playback Engine
  • Audio to Vibe
  • PWM input with 0% to 100% Duty-Cycle Control Range
  • Hardware Trigger Input
  • Built-in Waveform Sequencer and Trigger

And that is just to name a few. See the DRV2605L datasheet for a complete list.

Required Materials

You'll need a handful of extra parts to get the Haptic Motor Driver up-and-running. Below are the basic components used in this tutorial, if you want to follow along.

SparkFun RedBoard - Programmed with Arduino

DEV-13975
$22.50

Vibration Motor

ROB-08449
$2.95

Jumper Wires Premium 6" M/M Pack of 10

PRT-08431
$5.25

SparkFun Cerberus USB Cable - 6ft

CAB-12016
Retired

A microcontroller that supports I2C is required to communicate with the DRV2605L and relay the data to the user by means of vibration. The SparkFun RedBoard or Arduino Uno are popular options for this role, but just about any microcontroller development board should work. (The firmware examples use an Arduino library, if that serves as any extra motivation to use an Arduino.)

Arduino Pro Mini 328 - 5V/16MHz

DEV-11113
$11.25

SparkFun RedBoard - Programmed with Arduino

DEV-13975
$22.50

SparkFun SAMD21 Mini Breakout

DEV-13664
$24.95

Arduino Uno - R3

DEV-11021
$27.60

Suggested Reading

The DRV2605L is designed for a handful of uses. The Technical Documents provided by Texas Instruments includes application notes, user guides, literature and blogs. The DRV2605L communicates over I2C. We’ve got a great library to make it easy to use. We’re going to be using a breadboard to connect the breakout board to the RedBoard. If these subjects sound foreign to you consider browsing through these tutorials before continuing on.

How to Solder: Through-Hole Soldering

This tutorial covers everything you need to know about through-hole soldering.

Installing an Arduino Library

How do I install a custom Arduino library? It's easy! This tutorial will go over how to install an Arduino library using the Arduino Library Manager. For libraries not linked with the Arduino IDE, we will also go over manually installing an Arduino library.

How to Use a Breadboard

Welcome to the wonderful world of breadboards. Here we will learn what a breadboard is and how to use one to build your very first circuit.

I2C

An introduction to I2C, one of the main embedded communications protocols in use today.